Part Number: TLV61048 Hi, Team.
i've been asked by Customer as below.
Q1
when IC goes current limit, what type of current limit behavior IC would do? (cycle by cycle?)
Q2.
Customer has thought that PFM mode in its datasheet looks like burst mode…
Part Number: TLV61048 Other Parts Discussed in Thread: TPS61022 Can Input=3.5-4.35V achieve output=5V in TLV61048 ? if can , What is the maximum output current ? Thanks !
Part Number: TLV61048 Other Parts Discussed in Thread: TPS61372 Hello,
I've a problem in my project in which I'm using a TLV61048 to boost my voltage from Vbat(3V7) up to 5V or 12V, depending on the S6 switch position.
My board without the TLV61048…
Hi Charlie,
TLV61046A and TLV61048 are not p2p compatible. So please don't just drop in the TLV61046A instead of the TLV61048.
Following is the schematic for generating +/-25V based on TPS61046, which applies to TLV61046A as well.
The diode D7 and D8…
Part Number: LM5158 Other Parts Discussed in Thread: TLV61048 , Hello TI Power experts,
We are intending to design a boost/inverting dc/dc stage with a negative and positive output.
Vin: 9V
Vout1: 16V
Vout2: -16V
Iout_max: 0.5A
We have considered the…
Part Number: TLV61048 Hi Team,
My customer would like to know the current when this IC become PFM mode.
Datasheet said "When the FB voltage hits the PFM reference voltage, the TLV61048 goes into power-save mode".
However, I cannot find any information…
Part Number: TLV61048 Other Parts Discussed in Thread: TPS61023 Now we testing tlv61048 and have some problem.
test condition : use Li-ion Battery(3.7~4.2V), output=5.2Volt, 600mA
1. Output Enable : Even if the enable signsl is set low, the output remains…
Part Number: TLV61048 Tool/software: WEBENCH® Design Tools Hello,
I'd like to do WEBENCH simulation for TLV61048 but can't find it on ti.com.. Hasn't it been released yet or is there any good alternative solution to simulate it?
Thanks in advance…
Hi Abe san,
abe yusuke said: Is it possible that VREF varies between VREF-min and VREF-max at 25℃ ?
Generally, the VREF may varies between min and max within the whole temperature range. But it's very stable at one specific temperature.
When you use …
Part Number: TLV61048 Other Parts Discussed in Thread: TPS61087 , TPS61089 , TPS61088 Hello,
I have a 12V motor that I need to drive from three 'C' cells; nominal total voltage 3.3V-4.5V. I see the EVM design is for 12V out, 2.65V to 5.5V, which is very…