Part Number: TLV61070A Other Parts Discussed in Thread: LM5155 I am working on a design using the TLV61070.
My PCB consists of the regulator, MCU, and amplifying circuit and t he only sources of noise are buzzers and microphones.
In my PCB, most of…
Part Number: TLV61070A Other Parts Discussed in Thread: TPS61022 , TPS61033 Tool/software: Hello, I am using the TLV61070ADBVR with a Li-ion battery input voltage between 3V and 4.2V. I would like to have a voltage of 5V at the output to supply a USB…
Part Number: TLV61070A Other Parts Discussed in Thread: TPS61023
Hello, I am planning to use the IC TLV61070A in boost mode for my new design.
Below is the requirement,
Input voltage : 1.5VDC to 3.2VDC
Output Voltage : 5VDC
Outlut current…
Part Number: TLV61070A I used the following design for TLV61070. I'm aiming to get 5V at the output by keeping the input voltage between 3.7V and 4.2V. But I couldn't get it. What advice do you give?
Part Number: TLV61070A Other Parts Discussed in Thread: TPS61021A , TPS61299 Hi team,
Our customer is looking for the device that is able to use below requirements:
Vin : 0.7V to 1.5V(AA battery)
Vout : 5V
Iout : 300mA
I search the device…
Part Number: TLV61070A Hello,
I am just sharing a working design as a reference for anyone who plans to use the TLV61070A as a DC-DC boost converter.
Aim: To build a 5V boost circuit. The VIN will be from a 3.7V (4.2V MAX) Li-ion battery and the expected…
Part Number: TLV61070A I drew schematic to see output of boost converter, according to the datasheet Vref must be 500mV and output voltage should be 5V as arranged. But I think FB is wrong, it gives wrong output voltage.
Part Number: TLV61070A I designed the circuit as follows. I used a 2.2uH inductor with a 19mohm DCR and a 4.9A Isat, and added a 220pF capacitor to the feed forward path for stability. However, it cannot provide a 5V, 1A output at a 2.7V input; the output…