Part Number: TLV61220 Other Parts Discussed in Thread: TPS61099 Hello,
I have been developing with part TLV61220DBVR on a low power application. This system is battery powered, has a minimum power consumption of 20/30uA due to a wake up routine of a…
Part Number: TPS61021A Other Parts Discussed in Thread: TLV61220 Normal condition: Vin = 1.5 V, Vout = 3.3 V. Fault condition: Vin = 3 V to 4 V.
Question 1: In the fault condition, can Vout be turned off (reduced to 0 V or below 3.3 V) by pulling the…
Part Number: TLV61220 Tool/software: We use TLV61220 to get the power supply voltage (3.3V).
According to the datasheet, we calculated the voltage and obtained 3.53V.
Then, we changed only the inductor from "VLF4012AT-4R7M" to "VLS3012HBX-4R7M", …
Part Number: TLV61220A Other Parts Discussed in Thread: TLV61220 Is there any other difference to the TLV61220 besides the specification of the shut-down current? Will the TLV61220 be available in the furture?
Part Number: TLV61220A Other Parts Discussed in Thread: TLV61220 Tool/software: Dear Sir,
We are going to review the spec for TLV61220 and TLV61220A.
Here are some differences below, could you please check them and provide a update?
Thank you. …
Part Number: TLV61220 Dear Team,
Does TLV61220 can work at operating temperatures of -51 degrees?
If not, do you suggest us suitable solution? Thanks a lot.
Many Thanks,
Jimmy
Part Number: TLV61220 Other Parts Discussed in Thread: TPS61299 , TPS61099 , TPS61070 Tool/software: Hello,
I am using a TLV61220DBVR in circuit and am having problems with input current instability.
Vin = 1.4V, Vo = 3.3V, Io = 25mA max. AA lithium…
Part Number: TLV61220 Other Parts Discussed in Thread: TPS61299 , TPS61099 , TLV61070A , TPS61299A Tool/software: Hello,
We are currently using the TLV61220 in a new battery powered project. We see a similar issue to that reported in the related thread…
Part Number: TLV61220 Thank you for your help.
For the 4.7uH coil that connects between the SW and VBAT pins of the tlv61220, What is the recommended DC resistance value (DCR)?
thank you.
Part Number: TLV61220 Tool/software: Hi Ti
When I was designing the TLV61220, I found that the quiescent current at the input end of the chip is too large, when Vin=1.2V, Vout Noload, the input current is about 25uA when tested with Powermonitor.
…