Part Number: TPS62067-Q1 Other Parts Discussed in Thread: TLV62065-Q1 Hi,
The customer is considering changing TLV62065-Q1 to TPS62067-Q1.
Please review whether TPS62067-Q1 can be used for the existing schematic.
[TLV62065-Q1 Schematic]
Q1. Do not use…
Part Number: TLV62065-Q1 Tool/software: WEBENCH® Design Tools Hello:
Use the official website pspice model-SLIM249B.ZIP (110 KB) - PSpice Model
Simulation conditions:
Simulation 1:Change R10 and R11,All other parameters remain the same,Starting the simulation…
Part Number: TLV62065-Q1 Other Parts Discussed in Thread: TLV62065 , Hi Sir,
Customer is asking the difference between TLV62065 and TLV62065-Q1?
It is clear that the biggest difference is automotive grade and thermal performance, but they would like to know…
Part Number: TLV62065-Q1 HI Team,
My customer is requesting the whole temperature range(-40-125C) PFM mode VREF accuracy? In our datasheet it only spec a 1% typical value for room temperature.
For PWM mode, the accuracy is +-2% max and min, 0% typical…
Part Number: TLV62065-Q1
Hi Team,
Customer met a very strange problem and now it could be solved. But we really want to figure out the reason.
Customer use TLV62065-Q1 to change 5V to 1.35V.
As first they use resistance (100k and 10k) to divide the voltage…
Part Number: TLV62065-Q1 Other Parts Discussed in Thread: TLV62065 Hi team,
This is Jessica, glad to work with you.
Since customer want to do some evaluation about our TLV62065, could you please kindly help to provide us with the detail parameters of the…
Part Number: TLV62065-Q1 Other Parts Discussed in Thread: TPS62065-Q1 Hi all,
I would like to know that the device is capable to output 0.8V (0-2A) from 5V input in fixed frequency PWM mode. Do you have any data that shows the device is capable or any…
Part Number: TLV62065-Q1 Other Parts Discussed in Thread: TLV62065
Our customer is considering to use TLV62065-Q1.
They found about 100kHz oscillation at output in PWM mode.
I attached thier circuit and waveform.
Please let us know why 100kHz oscillation…
Other Parts Discussed in Thread: TLV62065-Q1 , TLV62065 Our customer consider to use TLV62065-Q1.
They get data of Phase margin,Gain margin.Please see attached.
TLV62065-Q1 Phase margin_Gain margin.pptx
Power save mode :Phase margin:41.7deg,Gain margin…
Other Parts Discussed in Thread: TLV62065-Q1 Hi Team,
I would like to use the TLV62065-Q1 to drive a load with the following conditions:
Vin: 5V
Vout: 3V3
Iout: 305mA
load capacitance: 95uF
Will the TLV62065-Q1 be able to drive a load with that high of…