Part Number: TLV62080 Team,
I would like to ask you if application note of SLVA494A can apply to TLV62xxx as well as TPS62xxx?
Best regards,
Hideyuki Takisawa
Part Number: TLV62080 Hello,
Please tell us about TLV62080.
The soft start is 10mV/us written in datasheet.
Do you have min / max parameters?
My customers want to know the approximate range.
Thank you.
Other Parts Discussed in Thread: TLV62080 , TLV62568 If there Maximum rating of transient SW pin voltage, please let me know.
-----------------------------------------------------------------
【Background】
・MP2159A is described below datasheet P3. (-1.5V…
Hi,
I need to know how these parts behaves on the output if set to nominal 1V8 and the load produce a short pull-up to 3V3 (about 150mA)? Will the controller allow the voltage to rise or fight back and keep 1V8? I assume that this condition firstly cause…
Other Parts Discussed in Thread: TLV62080 , TLV62084 Dear Sir
We have test turn on TLV62080 in 5Vin 2.5Vout/1.2A. the out rise waveform is smooth.
but when we modify EVB let output is 1.2Vout/1.2A.(Vin also 5V and just change FB resistor). the output rise…
Other Parts Discussed in Thread: TLV62080 Hi all, Would you mind if we ask PG operation of TLV62080? The datasheet shows as followings; -The power good maintains high impedance once the output is above 95% of the regulated voltage, and is driven to low once…
Other Parts Discussed in Thread: TLV62080 Hi all, Would you mind if we ask TLV62080? Usually, IL(inductor current) is the following; -IL=Iout(max)+ΔIL/2 So, when we choose the inductor, we consider ILIM value, we have to choose 2.8A's inductor. If…
Other Parts Discussed in Thread: TLV62080 Hello
PG terminal of TLV62080 is written connecting to the SW terminal in datasheet.
But if PG terminal connect to VIN terminal, how does PG operate?
Best regards,
Yokota
Other Parts Discussed in Thread: TLV62080 , TLV62090 , TLV62084 Hello, The TLV62080 current limit is 1.6A(min) and soft start is 100us(typ). If we use the TLV62080 with Cout=65uF, Vout=3.3V,Vin=5V, Iout=1A. At this condition, the inrush current will be 2.1…