Part Number: TLV62084 Hi Team,
Could you please kindly help test Vout ripple at below conditions? Thanks.
VIn = 3.6V, 3.8V, 4.2V
Vout= 2.8V
Iout=100mA
L= 1uH, Cout= 10uf + 22uf, 6.3V, 0402 package. effective capacitance is 40%* nominal cap value…
Part Number: TLV62084 Hi Sir,
My customer using TLV62084 would like have Vo=3.3V but looks a little bit issue about accuracy.
Would you pls advise how we can improve accuracy? thanks.
Thanks, Ian.
Part Number: TLV62084 Other Parts Discussed in Thread: TPS62825A , TPS62A02 Hi Team,
just want to check if there is FPWM version of TLV62084 or if there is trim bit to make TLV62084 into FPWM version. Thanks.
Customer need small output ripple but…
Part Number: TLV62084 Hi team,
My customer wants to know the minimum value of Vin when Vout is 2.8V, thus they need to know the maximum value of High side MOS Rdson. In datasheet it only shows the typical value, which is 120mohm.
Best Regards,
…
Part Number: TLV62084 Hi Team,
just want to check if there is data or curve on Frequency vs load @ Iout<0.2A, Vout=2.8V.
datasheet only show curve @ Iout>0.2A. Thanks.
BRs
Given
Part Number: TLV62084 Dear Sir,
TLV62084DSGR have a "SLO" marking on the IC top side
but i found some "-" marking at up and down the"SLO", and different IC have different position
could you please let me know the "-" marking mean? (date code or…
Part Number: TLV62084 Hi Team,
customer has a question
EN may have some noise, so EN may have some drop.
1. in datasheet, VIL=0.4V max, but if EN drops from 1V to 0.8V, what's the status of TLV62084?
2. Is there deglitch time on EN pin?
Thanks…
Part Number: TLV62084 Hi Team,
just want to double check with you if the soft-start time can be changed when Vout is fixed through external parameters.
#1 Datasheet mentioned that its Vout ramp slew rate is fixed, so the soft-start time at a fixed…
Part Number: TLV62084 Hi Sir,
We are doing for open/short test.
If possible damage chip cause Vin 5V into EN pin if take away R14 (for FB)?
Chip is damage now...