Part Number: TLV62090 Helo,
I'm looking information regarding longevity policy for TLV62090RGTR. How long this device will be available on the market?
Thank you,
Andrey
Part Number: TLV62090 Hello to whom it may concern,
I'm talking about SW voltage of TLV62090. When our customer evaluateing EVM board, they have some questions.
It seems that it exceeds the absolute maximum rating at the evaluation result that they…
Part Number: TLV62090 Hello,
Could you please let me know the min/max switching frequency at heavy load? According to the datasheet figure 3~6 , is the fsw(min) about 1.1MHz and fsw(max) about 1.5MHz? Best Regards, Ryuji
Part Number: TLV62090 Other Parts Discussed in Thread: TLV62085 Team,
I have a customer who is interested to know what the transition time of the PG pin is on the TLV62090. Do we have any characterization data for this available? Also, he also wishes…
Part Number: TLV62090 Other Parts Discussed in Thread: TPS62090 Hi all I would like to know the behavior of TLV62090 when DEF pin is low or floating. I think TLV62090 and TPS62090 are same die,so switching frequency of TLV62090 set 2.8MHz. You don't guarantee…
Other Parts Discussed in Thread: TLV62090 Hi all, I saw Absolute Maximum Ratings of TLV62090. SW absolute range is 0.3~Vin+0.3V. However PWM and PFM Operations of Vsw is about -1.8V under voltage. Is this operation wave AC wave? Please tell me the AC…
Other Parts Discussed in Thread: TPS62090 , TLV62090 Hi all. I would like to get accutual effiency data. The input and output condition is the following .
TPS62090 and TLV62090 efficiency comparison ■Test condition 1 Input 3.3V Output 1.2V / 0A~2A …
Other Parts Discussed in Thread: TLV62090 Hello
Is there a maximum limit value about TLV62090 SSpin capacitor?
Our customer is setting 72nF at SS pin.
Is there any concern about this setting value?
Best Regards,
Mayumi Tanemura