Part Number: TLV62130 Tool/software: Hi, TI expert
The customer applied the TLV62130 to two products with different input voltages(5V, 12V).
Product_1) Vin=5V: No problem
Product_2) Vin=12V: The IC dead due to a progressive failure.
In other words…
Part Number: TLV62130 We are AMPACS Corporation, a contract manufacturer, and the end customer is Logitech. Logitech is currently conducting a survey on wafer information for materials.
Please help provide the information for the materials listed below…
Part Number: TLV62130 Tool/software: Hi
I have been reviewing the datasheet of the TLV62130, and I have two questions about the SW Pin .
・Question 1 I tested the SW pin, and the waveform obtained is consistent with that shown in Figure 35 (Power…
Part Number: TLV62130 When a 5V power supply is input, for different TLV62130RGTR chips, some chips have a feedback pin output voltage of 0.84V, causing the output voltage to reach 3.5V, with a transient of 200mV.
Part Number: TLV62130 Other Parts Discussed in Thread: TPS62110 Hi TIer
Do we have a chip which pin2pin TLV62130 and its output voltage include 7V?
Customer want to find a chip like this. I do not find it on Ti .COM.
I think the current advanced…
Part Number: TLV62130 Other Parts Discussed in Thread: TPS54620 Tool/software: The TLV62130RGTR is used to generate a voltage of 1.8V, while the TPS54620 before it generates a voltage of 1.0V. 1. The TPS54620 is operating normally, generating an output…
Part Number: TLV62130 Tool/software: Hello,
My customer is having an issue where they have a few failures with the TLV62130 buck device where the output stage MOSFET has failed in a short circuit. The failure has occurred in both the upper leg -and…
Part Number: TLV62130 hi
i made a board using TLV62130.
20 board are being tested in field.
2 board is not work TLV62130.
no output on the TLV62130.
sw pin is not working.
It works by replacing the TLV62130.
below is circuit
below is…
Part Number: TLV62130 Hi team,
Customer is checking the package size with us, could you help provide the spec of the marked corner place?
Thanks and Best Regards,
Will
Part Number: TPS563206 Other Parts Discussed in Thread: TLV62130 , , TPS62903 Tool/software: Hi, Ti power management team
Can i replace the TLV62130 in the following two scenarios:
Application
MCU Power
Voltage / Current : 3.3V / 100mA …