Part Number: TLV62130 We've been using TLV62130 for many years now in multiple devices, not giving problems.
The protoboards of our latest devices all worked fine.
Validation of the final PCB was done, all OK.
Now after putting the first batch of …
Part Number: TLV62130 Other Parts Discussed in Thread: TPS61253A , TPS62933O Hi, Team
My customer is looking for a Buck DCDC, Vin 20-25V, Iout:2-3A, Vout:5V
But since the project is use in portable smart speaker with 2 cells battery, they prefer the DCDC…
Part Number: TLV62130 What is the behavior of the TLV62130 under the following conditions / What output showed under following condition:
a) When Input capacitor between PVIN to PGND is short circuit?
b) When R2 (on FB pin) is short circuit?
Assume that…
Part Number: TLV62130 Other Parts Discussed in Thread: TPS62903 On another device that returned 'dead', we noticed again a low voltage on the EN pin: 0.48V when pulled up to Vin@5.0V over a 1K resistor. This indicates a much higher current than…
Part Number: TLV62130 Dear,
According to the datasheet, the pins of the schematic diagram TLV62130&TLV62130A are compatible, but the effective output states of PG are different. I would like to confirm whether these two materials can be completely replaced…
Part Number: TLV62130 Hi team,
My customer use 4pcs TLV62130 in their project, below is the schematic.
As shown in below figure, when the TLV62130(12V to 3.3V) is turn on, it appears that 12V power is being affected, causing the 1.8V to have an overshoot…
Part Number: TLV62130 Hi,
It is used at VOUT = 2.5V.
Looking at the TLV62130 datasheet, the PG has a 100kΩ pull-up resistor mounted.
We are considering reducing this pull-up resistance to 100 kΩ or less. Therefore, I would like to know the…
Part Number: TLV62130 Hi team, I'd like to know about setting for the webench. TLV62130 can output 5.5Vmax. This has been updated in the datasheet in the past. The Webench has a 5Vmax, when will it be updated? And, it seems that the minimum value of soft…
Part Number: TPS62130A Please check following compare products website.
compare products
I think some features have been deleted or erroneous.
Would you please fill in the yellow highlighted cell in the attachment?
6825.comparison.xlsx
Regards,
Part Number: TLV62130 Dear Team
Good day!
Our customer use the TLV62130 in their application , there are 2 devices are burning when they working , the customer check their board and found There's something wrong with the SS/TR pin cap welding , it is…