Part Number: TPS62130 Other Parts Discussed in Thread: TLV62130 What is the difference between TPS62130 and TLV62130? Is it the same? Can I replace them with each other?
Part Number: TLV62130
Hi, I've the following circuit set with the 5.25v output. The input also has 8 x 220uF solid polymer caps (not shown). The inductor is a coilcraft 5030. On the oscilliscope I can see the light load pattern. AC coupling shows about…
Part Number: TLV62130 Dear all,
My customer used TLV62130 in their case. The EE is a charging base for their tablet. The simplified block diagram is like below:
In normal operation, when they attach the tablet to the charging base through pogo pins, the…
Part Number: TLV62130 Hello,
I a design, a TLV62130 is used to create a 3.2V voltage supply.
Probing the SW pins I see the waveform below during operation.
I am wondering why there is this sine waveform before the square pulse.
Any idea ?
Best regards…
Part Number: TLV62130 Other Parts Discussed in Thread: TPS62135 , TPS62147 , , TPS62130 , TPS3703 , TPS3890 Hi team,
As my input voltage ramps up with very slow slew rate 1V/s, the ramp rate at the output is concerned.
So, I'm considering to control the output…
Part Number: TLV62130
Hi support team,
It is used with 12V input and 3.3V output. However, when the load is light (probably a few mA), about 3.6V is output. Do you know what caused it?
When a load current of about 15mA is applied, it stabilizes at 3.3V…
Part Number: TPS62813-Q1 Other Parts Discussed in Thread: TPS62813 , TLV62130 Hi team,
TPS62813's R_θJC(top) and R_θJB are all lower than TLV62130. But its R_θJA is higher than TLV62130. That's why?
How to compare the thermal performance…
Part Number: TLV62130 Here in my company we are using MYIR z-turn board. On that board they used TLV62130 to convert 5 v to 3.3 v. There are two types of powering is available one is USB and another one is 5v adapter. While using the USB powering, it works…