Part Number: TLV62130 Hi,
could you give suggestion that can meet below requirment:
Vin 10V
Vout:5V/2A and 3.3V/2A
Iq<10uA
I find the TLV62130 can meet the requirement, but the cost is higher. do you have other recommendations? thanks.
Part Number: TLV62130 Other Parts Discussed in Thread: TPS62130 , Hello Team,
The customer would like to confirm the PSPICE model.
Is it possible to use the "TPS62130" PSPICE model for the "TLV62130" transient simulation?
Thank you…
Part Number: TLV62130 Hello experts,
I got question for current consumption at no load from customer.
With TLV62130EVM-505, customer set 12Vin and 5Vout.
At no load, input side current is above 10mA. It looks not only Iq.
Do you have any idea for the…
Part Number: TLV62130 Tool/software: WEBENCH® Design Tools I posted following question. But the answer was irrelevant.
I'm not talking about measurement ringing due to long probe lead. I'm talking about input capacitor.
Does anyone give me the…
Chris-san,
Thank you for replying.
My concern is output spike, its frequency is about 250MHz. FAQ_2.pdf
The video mentions for a very short time, "Make this routing by your self and keep shortest possible, low impedance as possible".
Let me…
Part Number: PMP9802
Hi,
I need to design a circuit that looks similar to the one in PMP9802. I have, hence, been studying the material and how the design works and have a question regarding its functionality. As far as I understand, the whole concept…
Part Number: TLV62130 Other Parts Discussed in Thread: TPS62133 , , Hi,
I'm experiencing a problem with PG pin of the TLV62130. As per manual: 'With TLV62130 it is high impedance when the device is turned off due to EN, UVLO or thermal shutdown.' In my…
Part Number: TLV62130 Dear All,
I designed an inverting power supply circuit of TLV62130 for -5V power supply.
Non-inverting power supply circuit working was perfect, but there was an abnormal output voltage problem on the inverting power supply circuit…
Part Number: LP873220 Other Parts Discussed in Thread: TPS22965 , TLV62130 I have sent a question on this link before, but this engineer did not answer in detail, can you look at it, explain it to me in detail, why “Using TLV62130 in place of TPS22965 will…