Part Number: LP873220 Other Parts Discussed in Thread: TPS22965 , TLV62130 I have sent a question on this link before, but this engineer did not answer in detail, can you look at it, explain it to me in detail, why “Using TLV62130 in place of TPS22965…
Part Number: TLV62130 Support Path: /Product/Development and troubleshooting/ Hello TI-Team,
we are using 3 TLV62130 to produce the power for a xililx FPGA. The first produces the core power (1.0V) and after he ramped up,
he starts the second TLV62130…
Other Parts Discussed in Thread: TLV62130
Customer has designed in a TI TLV62130 DC-DC converter for a line card project. They are currently having some failures where the bottom MOSFET is failing short at about a 10% rate on the prototype line cards…
Other Parts Discussed in Thread: TLV62130 I have a circuit using the TLV62130 to charge a battery. The input voltage is 5.0V and output is 4.0V. The input current is 1.5A, and the output current is 1.5A. I expect the efficiency to be a little higher.…
Other Parts Discussed in Thread: TPS62130 , TLV62130 Chris Glaser
I notice that datasheet of TLV62130 said TPS62130 has improvered features. But it is difficult to find the difference between TLV62130 and TPS62130. So, could you please show me the improved…
Part Number: TLV62130 Tool/software: WEBENCH® Design Tools When I design TLV62130 circuit with WEBENCH, the default lowerbound and upperbound of inductor IDC is 5.506A and 10A.
How is this value decided? Does it consider TLV62130 current limit value…
Other Parts Discussed in Thread: TLV62130 , TLV62150 Hi,
I measured output ripple voltage as below and then the high frequency noise on ripple noise. I think this is not specific for TLV62130 because I remember to see this kind of waveform at other…
Other Parts Discussed in Thread: TLV62130A , TPS62130A , TPS62130 , TPS62080 , TLV62130 Hi, Could you tell me about TLV62130A vref voltage min max? Customers want to assess the output voltage accuracy. Best regards, Yusuke
Thanks again for clarifying and continuing to dialogue on this issue.
The issue with inductance in the output leads is the ringing created. Instead of just Vout and GND, now you have an LC circuit which can ring up and down--above 5V and below GND…