Part Number: TLV62130A
Hi,
We got a question from customer about TLV62130A. Could you help us?
[Question] How much is the maximum delay time between "the voltage is applied to EN" to "the IC will start switching"? They don't need guarantee. They…
Part Number: TLV62130A Hi,
We got a question from customer about TLV62130A. Could you help us?
[Question] Our customer is considering adding schottky barrior diode from PGND to SW for improving efficiency. Is there any concerns in this usage?
…
Part Number: TLV62130ATLV62130A - Voltage of VOS-pin
Hello.
The following sentence is on the page-14 of SLVSB74G.
9.2.2.2 Programming the Output Voltage "In case the FB pin gets opened, the device clamps the output voltage at the VOS pin internally…
Part Number: TLV62130A I found below description in datasheet P14.
"In case the FB pin gets opened, the device clamps the output voltage at the VOS pin internally to about 7.4 V."
When they use this part VIN:5V and FB pin gets opened,please let…
Other Parts Discussed in Thread: TLV62130A Hi,
My customer has question about TLV62130A. Could you tell me about questoin?
[Question] - Is there any sequence requirement between EN and FSW? My customer considers to input High signal to EN and FSW…
Part Number: TLV62130 Other Parts Discussed in Thread: , TPS82130 Is there a minimum load current requirement for TLV62130 stability?
What are differences between TLV62130 and TLV62130A? Sometimes I see a different reference voltage for parts with a…
Part Number: TLV62130A Hi,
We got a question from customer about TLV62130A. Could you help us?
[Question] When PVIN, AVIN and EN is open, 6V is applied to Vout from external power supply. Please see below figure.
- Is there any concerns about this…
Other Parts Discussed in Thread: TLV62130A Hi,
My customer has question about TLV62130A. Could you tell me about questoin?
[Question] - My customer considers to use TLV62130A under the folowing condition.
Vin=6V to 10V Vout=5V Iout=1.6A max fsw…
Part Number: TLV62130A Other Parts Discussed in Thread: TPS62130A Dear team,
Could you please help me with the following two questions ?
Thanks a lot !!
TLV62130A datasheet recommend a 5Vout max, I suppose this includes the resistors tolerance…