Hi Marco,
On the TLV devices, there are only TLV62130 and TLV62150 but there is no TLV62140. Can you confirm what part numbers are you trying in WEBENCH? I can check out the tool with those two part numbers.
Thanks,
Amod
Other Parts Discussed in Thread: TLV62150 Hi
I have used TLV62150, for 5 Volt OUT Option. My input is 12Volt & Output is 5 VOlt. When i connect a load it consume lot of current in losses and i am getting lower efficiency of the Converter.
Can you please…
Other Parts Discussed in Thread: TLV62150 , TPS62150 Dear support member,
My customer used TLV62150.
Output voltage range of TLV62150 has become 0.9V ~ 5V.
When output voltage 5V, Can you use the DEF pin high? 5.25V (5V + 5%) is more than output voltage…
Other Parts Discussed in Thread: TLV62150 Please let me know about absolute maximum rating of TLV62150 SW pin.
It is written in datasheet -0.3V to Vin+0.3V. However I think it is difficult to limit the overshot and undershoot of SW pin within this range…
Part Number: TPS2121 Other Parts Discussed in Thread: TPS22913 , TLV62150 Dear Team,
Our customer have a project with dual input .
They use TPS2121 for oring circuit.
Power input as the below.
USB 5V@3A
2.Battery 6V~8.4V @2A
They hope default input is…
Other Parts Discussed in Thread: TPS62150 , TLV62150 1. Could the TPS62150 replace the TLV62150? (fot 9V input and 5V or -5V outputs).
2. Regarding the control inputs SS/TR, DEF and FSW in -5V or -3.3V circuit: (a) In the TLV62150 data sheet, figure 40…
Part Number: TPS62130A Other Parts Discussed in Thread: TLV62150 Dear Specialists, Customers need FMEA information to adopt new parts. Please tell me the FMEA information of TPS62130A and TLV62150. It helps in design-in.
Best regards, Yusuke
Part Number: TLV62565 Other Parts Discussed in Thread: TLV62084A , TLV62150 Hi there
is there any TI device similar to TLV62565 , but the Iq of which will be smaller than 30 uA .?
My requirement would be : Vin = 5.5V Vout = 1.2A Vout 3.3V SOT 23-5 , …
Other Parts Discussed in Thread: TLV62130 , TLV62150 Hi,
I measured output ripple voltage as below and then the high frequency noise on ripple noise. I think this is not specific for TLV62130 because I remember to see this kind of waveform at other device…
Other Parts Discussed in Thread: TPS62150 , TLV62150 We are working of a battery powered device which will mostly be turned off so micro amperes of current is what we need during power down. We are considering TLV/TPS62150 DCDC converter due to their high…