Part Number: TLV62568 Hi team,
One of my customer will use TLV62568.
They measured switching frequency and TLV62568 showed 2.4MHz switching as these captured waveforms whereas its datasheet sates fsw is 1.5MHz(typ).
5Vin/3.3Vout/Iout=156mA
5Vin/1.2Vout…
Part Number: TLV62568 Hi team,
Our customer is considering TLV62568 for interface IC to input core and PHY voltage and also have concerned about the EMI noise.
Are there any data of EMI measurement ?
Thank you and best regards,
Michiaki
Part Number: TLV62568 Dear Team,
What is the max Rds_on of the high-side FET depending on Junction temp? I would be interested in Tj from 85 to 125 at Vin 3.3V. Doesn`t have to be exact.
Regards
Andreas
Part Number: TLV62568 Hello experts,
The TLV62568DRL data sheet states that the soft start time at Tj = 25 ° C is 0.9ms (typ). Please tell me the soft start time min value / max value when Tj = -40 to 125 ° C.
Soft start time (Tj = 25 ℃) Typ…
Part Number: TLV62568 Tool/software: WEBENCH® Design Tools Hi Team:
can you provide the simulation model for TPS62568 Loop simulation, there is a Pspice Transient model in the website and Webench, can you help to provide the converted SImplis model for…
Part Number: TLV62568 Other Parts Discussed in Thread: TLV62130A I am now using TLV62568 in my mass production design, and there is a new request for auto discharge.
I want to use the PG pin of TLV62568P to implement auto discharge,
From TLV62130A datasheet…
Part Number: TLV62568 Dear
Recently, TLV62568 was found O/S issue, and it was found that the die shapes of NG and OK are different under x-ray, as shown in the attachment. Please help confirm whether there are two kinds of dies in TI TLV62568, so that…
Part Number: TLV62568 Hi team,
my customer measure gain/phase performance and gain margin and phase margin can pass with Cff=6.8pF
Below is their bode-plot result, and can you explain why there is rapidly drop then jump waveform around 300k~400kHz?
Is…
Part Number: TLV62568 Hi team,
We are testing the light load transition report for customer and they have some concern about our power save mode.
They are asking to test the point of PSM into normal mode as below figure.
It shows the transition point…