Part Number: TLV62569 Other Parts Discussed in Thread: TPS55010 Hi,
Customer wants to use the following circuit. He wants to replace inductor to transformation, because of supporting Isolation-DC/DC. Can this device support it?
If no, please let me…
Part Number: TLV62569 Hi ,
In datasheet, when using 1uH inductor, 2x22uf need to be used.
As you know, there are p2p solution from other vendors, they can use 1uH+1x22uf (0603) or 2x10uf (0402). Please kindly check if we can also use this. Thanks.
BR…
Part Number: TLV62569 One question to 7.3.4 Switch Current Limit in datasheet. Could you advise what value of the current limit is? 2A? Is "peak current detect" enable when startup or stead status?
Part Number: TLV62585 Other Parts Discussed in Thread: TLV62569 , Hi Team,
could you please provide Efficiency comparison between TLV62569 VS TLV62585 based on Condition: Vin=4.5V Vout=1.1V L=2520 size.
Thanks!
Patty
Part Number: TLV62569 Other Parts Discussed in Thread: TLV62585 , TLV62568 , Hi TI team,
TLV62569 is suitable for my application, but I see TI recommends some alternative parts (refer http://www.ti.com/product/TLV62569 ). Before moving to mass production…
Part Number: TLV62569 Hi Team,
What happens if we have TLV62569P (PG version) SOT563 and the PG pin is tied directly to an output voltage <5.5V?
Is this safe behavior for our device?
What would be the additional power dissipation within the device…
Part Number: TLV62569 Dear team,
Customer calculate the Tj with Ta=86 as below picture shows, it seems that the IC has reached the temperature protection limitation. Could you kindly help me correct?
Thanks.
Best regards,
Sammi
Part Number: TLV62569 Hi TI,
I would like to use the TLV62569 for my product. The datasheet indicates that the switch frequency is 1.5MHz. Do I have to use an input EMI filter for this buck converter? Because of, the switching frequency is above 150KHz…
Part Number: TLV62569 Dear Sir/Ms.
My client asked me this question, I did not see these parameters when I looked at the datasheet (Chapter 6.5). Could you tell me what is the input current IIL /IIL of EN Pin?
Best Regards,
Kami Huang
Part Number: TLV62569 Other Parts Discussed in Thread: TPS62825 Hi All,
I would like to replace competitor solution by using TLV62569, but TLV62569's switching frequency is only 1.5MHz(2.2uH) and competitor is 2.5MHz (0.47uH)
Customer wouldn't like…