Part Number: TLV62569A Hi team, I'd like to know about output capacitance. My customer wants to use add 630uF(an aluminum electrolytic capacitor) for it is a measure for a momentary power failure. Can it use? Sincerely. Kengo.
Part Number: TLV62569A Hi team,
can you please provide some insight on the expected min and max values for the input leakage current into the FB pin (I_FB) for both the TLV6256 9 ADRLR and the TLV6256 8 APDRLT across full operating temp range?
my customer…
Part Number: TLV62569A Hi,
My customer used two TLV62569A in their speaker products. 5V usb in, 3.3V and 1.8V output. so far, they failed in EN55032 radiated test. I know it is a systematic problems. just help to see if TI part have potential issue. appreciate…
Part Number: TLV62569A Hi ,
I see there's over current protection feature with this chip, but not sure if the function will automatically recovered or not if the current load is back to normal level. Would you double confirm this?
In parallel, there…
Part Number: TLV62569A I have two questions.
What is the maximum allowed Cout on the TLV62569A output? Customer has 91uF of Cout (before de-rating) with 1uH in 1.8V application.
Also, is there an ESD clamp on EN pin? What does the structure look like…
Part Number: TLV62569A Hi team,
Can I use any voltage up to 6V as PG pull-up supply?
According to Abs max in the datasheet, it looks OK, but if you have any concerns please let me know.
Regards,
Part Number: TLV62569A Other Parts Discussed in Thread: TPS62826A Dear TI,
Here my customer wants to evaluate TLV62569A in their case, the VIN range is from 3.4V`4.2V, the Vout is fixed 3.3V. They want to confirm if there is a concern when working under…
Hi Kayleigh,
Apology for the late reply.
I looks like this particular model cannot support TINA. Unfortunately, we still need to request our modeling team generate a TINA model to TLV62569A which will take 4 to 6 weeks minimum. Can the WEBENCH support…