Part Number: TLV62585 Other Parts Discussed in Thread: TPS62823 Hi Sir
I use TI website to search power solution ,TLV62585 show current mode ,is it correct ?
Thanks
Part Number: TLV62585 Hi ,
May I ask that why the junction to ambient of QFN is better than SOT, but the other parameter of SOT is higher than QFN package?
Thanks for your help.
Part Number: TLV62585 Other Parts Discussed in Thread: TPS62826 LPDC support team
Why does the thermal information between datasheet and Webench different?
The below is the thermal information in datasheet
The below is the thermal information in Webench…
Part Number: TLV62585 Hi,
I am going to use TLV62585 step down converter ICs to power up IMX6Q SoC. Therefore it needs a power up sequencing.
That means every other voltages need to be going to the SoC after giving the 3.3V to the SoC.
As mentioned in…
Part Number: TLV62585 Other Parts Discussed in Thread: TLV62568
Hi Team,
May I know the exactly condition of mode transition? by peak current? or more then that?
1. the exactly condition from PSM to PWM
2. the exactly condition from PWM to PSM
Thank you…
Part Number: TLV62585 Hi Pals,
Could I use output capacitor value 330uF+100uF for TLV62585 ?
I am worry about that it will trigger OCP function because the soft start is the internal function for TLV62585.
What is the max output capacitor value could I…
Part Number: TLV62585 Please let me know the "V" and "HR" decode in the package code VQFN-12-HR.
Thanks
Gan Chen Component Engineer Viking Technology, A Sanmina-SCI
2950 Red Hill Ave.
Costa Mesa, CA 92626
(714) 913-2200 x2209 (voice…
Part Number: TLV62585 Dear all
About Output Discharge function, I have two questions as below:
1. How many is current limit of Output Discharge FET Switch ?
2. How much maximum value of Vout cap that could be connected ? I want to connect with 470uF cap…
Part Number: TLV62585 Hi Experts,
In addition to using the feed forward capacitor , Is there any other way that could reduce the ripple voltage on PSM mode ?
My input is 3.3V, output : 1.2V/Max 0.75A, Normal is less than 0.2A.
Thanks.
Part Number: TLV62585 Other Parts Discussed in Thread: TPS62480 , TPS62180 Hi,
I need an alternative component with 5A output instead of using TLV62585 3A switching regulator.
Specially I need to output Vin as it is for power sequencing thing.
My requirements…