Hi Archie A.,
the shared waveforms does not help, all the measurements are done using AC coupling which only shows the noise and ripple,
Please provide me something like below, in DC coupling. All VIN to GND, SW to GND & VOUT to GND in same scope shot…
Part Number: TLV627432 Hi team,
in below link it mentioned there is transient spike in datasheet, but I download datasheet on website and seems no transient spec. Please kindly check.
TLV627432: SW pin absolute maximum ratings(AMR) AC value - Power management…
Part Number: TLV627432 Other Parts Discussed in Thread: TPS62840 Hello Sir:
TLV627432 is not enough for end customer application.
Please help to recommend P2P with RT5707WSC solutions for us.
And that output current should be over 600mA.
Looking forward…
Part Number: TLV627432 Other Parts Discussed in Thread: TPS62743 Hi team,
My customer wants to check if we have any solution that can output 0.6/0.65/0.9/1.3V with TLV627432?
If the answer for this question is no, do we have any BOM to BOM device with…
Part Number: TLV627432 Hi team,
My customer test OCP and the waveforms are attached. When it is shorted, the current keeps at 800mA and the output voltage is pulled down to 62mV. I know that OCP is achieved by cycle-by-cycle detection. But why does the…
Part Number: TLV627432 Hi team,
My customer test a -600mV on SW pin, it lasts for 40ns. In datasheet, it says the absolute maximum ratings value of SW is -300mV. I think it is a DC value, which means the SW pin can tolerate -300mV for a long time. And…