Part Number: TMS320F28062F Hi Team,
How to upgrade the motor control application developed based on F2806xF solution: instaspin_foc (proj_lab03a) to solution: universal_motorcontrol_lab (f28002x). What changes need to be made in the software part and…
Part Number: CC1312R Other Parts Discussed in Thread: UNIFLASH Hi, I generate a hex file by CCS and I try flash program on CC1312 thru XDS110 by SmartRF Flash programmer 2 v1.8.2. But, result is fail with "Unknown record type:3" error.
When I select…
Part Number: LP-CC2651R3SIPA Other Parts Discussed in Thread: CC2651R3SIPA I have a simple application that uses I2C and 2 switch input. When I try to leave CCS, only 1 of my launchPAD will run the program under a separate power supply. I purchase a n…
Part Number: TPS25750 Other Parts Discussed in Thread: TPS25751 Hi expert
my customer had a new project used PD, the max input is 20V/3A, output is 5V3A. we selected TPS25750. because of the European Union about (EU) 2022/2380. my customer need to test IEC62680…
Part Number: BQ76952 Hi team,
From the datasheet, when TS1, TS2, TS3 are configured for general purpose ADCe, the input voltage range is 0~1.8V(VREG18).
My customer wanted to know in this case, whether these pins are not pulled up by internal resistors…
Part Number: LM73100EVM Hi forum members,
I need to connect two power sources in parallel for getting redundancy with two independent power paths. To reach this goal I first thought about simple diodes to put in series to the sources' outputs for oring…
Part Number: LMX2594 In my application I am using full-assist for tuning to a set of frequencies and upon power up, the software will use no-assist tuning to determine and save the VCO SEL, CAPCTRL and DACISET values for each frequency.
In the data sheet…
Part Number: LOG101 Looking for some clarity regarding Burr Brown parts and their differences:
LOG100JP
LOG100JP-2
LOG100JP-3
LOG100JP-4
Please advise of the differences if possible.
Thank you,