Part Number: TLV7012 Hi team,
My customer would like to evaluate this device but there is no EVM in TI system.
So could you advise alternative EVM could be used?
Thanks
Part Number: TLV7012 Other Parts Discussed in Thread: SN74LVC1G17 Hi Team
My customer consider using a (window) comparator to provide an RC low pass (excited by one of your SN74LVC1G17) with a "hard" cut-off frequency. This means that…
Part Number: TLV7011 Other Parts Discussed in Thread: TLV7012
Hi team,
Regarding TLV7011, the absolute maximum rating for the input voltage is specified as VEE – 0.3 V to 7 V. Based on this specification, it appears that the device can tolerate an…
Part Number: TLV7011 Other Parts Discussed in Thread: TLV7012 Hi Team,
Can we connnect Vee to ground for TLV7011DCKR?
Not state in DS for TLV7011DCKR but TLV7012/22.
Thanks.
Part Number: TLV7011 Other Parts Discussed in Thread: TLV7012 , LMC555 , TLC555 , NE555 Tool/software: Hi team,
We want to add delay function circuit at the TLV7011 output end to get several ms delay. Do you have any suggestion circuit?
Part Number: LM2904-Q1 Other Parts Discussed in Thread: LM2904 , LMV358A , TLV7012 , LM393LV
When operating LM2904 opamp as a comparator, with Vcc 5V, and single supply operation, I am only getting 3.7V and 0V are my switching state, instead of expected…
Part Number: SN74LVC2G17 Other Parts Discussed in Thread: TXU0102 , TLV7012 I am looking for a Schmitt trigger buffer device with 2 channels which can handle 3.3V logic inputs and give 5V logic outputs with no error.
According to the datasheet for…
Other Parts Discussed in Thread: OPA2333P , TLV7031 , TLV7012 , TLV7011 , TLV7032 , TLV4051
Hi Sir,
My customer would like design OP with the following spec.
low Iq, like( less than 10uA per channel),
Vin is 5.5V max
Vin is 2.5V min
Push…
Swathi
If there is anything additional that we can help address in regards to the comparator, please let us know.
If using open-collector outputs is not suitable, you can always OR together two push pull output devices with a diode on each output…
The output frequency is affected by the voltages at which the inverter switches. The Schmitt-trigger inputs of logic devices have a wide variation of voltage thresholds (see the V T+ and V T− specifications in the electrical characteristics table). The…