Part Number: TLV7022 Other Parts Discussed in Thread: TINA-TI I am supporting an application using the TLV7022. The application has seen some concerning behavior during system-level noise testing. As we work through figuring this out, I need the following…
Part Number: TLV7022 Other Parts Discussed in Thread: LM293 , TLV7021 , TINA-TI Hi,
My customer is using TLV7022 as an input to the DSP and they found that the falling time of output (input of DSP) is about 2.7us and is longer than showed in datasheet,…
Part Number: TLV7022 Hi,
My customer is planning a use case at low current implementation for communication module using TLV7022. May I know if there is any adverse impact if the TLV7022 central thermal pad is floating (no PCB solder footprint) without…
Part Number: TLV7022 Other Parts Discussed in Thread: TLV9022 , TLV7021 Hi team,
Could you give me comment on following customer question?
Q1. Could you provide alternative options of TLV9022 for smaller size package? TLV9022 is still candidate, and they…
Good morning Norbert
I understand that you are not satisfied with our support. I am sorry that we cannot provide proprietary information on our ESD implementation on the TLV7022 and unfortunately that device cannot be used for your application. Other…
Part Number: TLV7022 Hi team,
I am attaching the schematics of TLV70228QDBVRQ1 , please review it and let me know your inputs. With regards,
Jayashree.
Part Number: LM393B Other Parts Discussed in Thread: LM339 , TLV4021 , TLV7042 , TLV7041 , TLV7021 , TLV7022 , TLV7081 , LM393LV , LM139 Hi,
My customer uses LM393B as voltage detection.
when there is input power and ambient temperature is at >0C, it works normally…
Hello Kunal,
As Clemens stated, the LM2903B is not a rail-to-rail input. The maximum input voltage is Vcc-2V, or 3V on a 5V supply.
The model is designed to fail if the input range is violated.
I would suggest trying the new LM393LV or TLV7022, which…
Part Number: LMC7221 Other Parts Discussed in Thread: TLV7022 , TLV9032 , LM393LV , TLV1805 , TLV9022 Could you please tell us if the output FET in the LMC7221 is a self-locking type?
Part Number: LM393B Other Parts Discussed in Thread: TLV7022 , LMP7300 Hi,
I have an application that compares (sorry, kind of obvious) two voltages, however the two voltages are independent of each other, there is no reference or fixed voltage to calc…