Part Number: TLV707 Hello TI team,
Are you all able to source the TLV707185PDQNR from outside of China? Or is it only produced in one of your China Fabs? Our client needs NDAA compliant parts. If not is there a similar product you can recommend that…
Part Number: TLV707 Hi Team,
We heard from my customer that when look into detail start up waveform of TLV707/742, they found that there will be an over spike at Vout. Please find below schematic and waveforms for TLV70712.
The input voltage is…
Part Number: TLV707 Other Parts Discussed in Thread: TPS7A20 Hello support team,
Customer ask if TLV707 has internal Reverse current protection between VIN and VOUT, because of abs max VOUT spec on datasheet. I assume that TLV707 has no reverse current…
Part Number: TLV707 Hello guys,
One of my customers is considering using TLV70726 for their next products. At this moment, they have the following questions. Could you please give me your reply?
Q. What is power up time of TLV70726 after VIN is powered…
Part Number: TLV707 Hello support team,
This is FAE Dave, thanks for taking time looking into this issue.
Figure.1 is the limit listed in datasheet and it states that the limit is 450mA of the maximum.
Fig.1
My customer has experienced the…
Part Number: TLV707 Hi all
My customer has below question.
Please comment / clarify.
Best regards
Ueli
-------------------------------
Dear TI Team,
According to datasheet (SBVS153F, May 2018), TLV707 has the following temperature range…
Part Number: TLV707 Hi Sir,
Here is spec. from TLV707, I got question for VIH definition, as you can see VIH is 0.9 to VIN, does it mean EN can’t higher than application VIN voltage or VIN recommend operating voltage2V~5.5V? if VIN=3V, EN=3.3, is any…
Hi Yuzhe,
TLV707 can have 5V output options, but the orderable current does not have this option listed. Some of the reason could be the demand for this voltage option is not high enough for us to release it as a catalog option. Please allow some time…
Part Number: TLV707 Hi Team,
My customer need to verify TLV70725. The questions are as below.
1. For bode plot test, could we directly add 10 ohm resistor on the output path? Or other suggestion resistor value?
2. How do we set the ripple injection…