Part Number: TLV710-Q1 Other Parts Discussed in Thread: TLV710 Hi Team,
We have used TLV7103318QDSERQ1 for SD card supply for our board, during the prototype phase the board was working with SD card booting. After some 100 board production we faced…
Part Number: TLV710-Q1 Hi Team,
We have used TLV7103318QDSERQ1 for SD card supply for our board, during the prototype phase the board was working with SD card booting. After some 100 board production we faced the issue that showing 1.1V instead of 1…
Part Number: TLV710-Q1 Tool/software: Hi team,
Does the TLV7103318QDSERQ1 have an internal pull-up or pull-down resistor on the EN pin? What does the Q in the part number mean?
Best Regards,
Jade Lan
Part Number: TLV710-Q1 Hi team:
Can the TLV7103318QDSERQ1 output1 and output2 be combined? It appears to be mirrored in block diagram. Input 5V, output1&output2 for 80mA
thanks.
Part Number: TLV710 Other Parts Discussed in Thread: PCA9306 Tool/software: I saw the TLV7103318DSET part in the PROC141E4_RP schematic.in that I have on doubt.
This IC has two enable pin's and the EN2 is high so OUT2 comes by default (VLDO_CSI_1V8…
Part Number: TLV710
We are using TLV7103318QDSERQ1 in our design for dynamic voltage scaling of SD card. This design is referred from the one used in Jacinto 7 EVM design . I have attached the schematic from our design. Please review and confirm the…
Part Number: TLV710 Hi Team,
We are using TLV7103318QDSERQ1 in one of our design. Can you please help us clarify that the absolute max value for the En pin is VIN + 0.3V.(VIN 0.3 is a typo).
Regards,
Gireesh
Part Number: TLV710 Hi team,
In the AM62x SK EVM's schematic, this device is used to supply both 3.3V and 1.8V selectively.
It look like EN2 is always high, and by controling EN1, it can switch the output of 3.3V or 1.8V
Does this device have…
Part Number: TLV710-Q1 Hi,
In the Jacinto7 EVM design, the 1.8V and 3.3V output of TLV7103318 are short with 0ohm resistors as shown in the figure below. And here is description that if we want to achieve 3.3V output, the EN1 and EN2 should be both…