Part Number: TLV716P Tool/software: Dear TI Engineer,
For the output voltage of TLV7163318PDPQR , we want to know which OUT PIN is output 3.3V and which OUT PIN output 1.8V, can you help confirm it?
Thanks,
Kind Regards
Part Number: TLV716P On the TLV716P3318 device I am assuming that the 3.3 v is on the Pin labeled OUT1 (1)
and 1.8v is on the pin label OUT2 (2). I would like to verify before releasing the design and I could not
find any documentation on this.
Part Number: TLV716P
Dear Sir/Madam,
Can I check if I want to use TLV716P with input voltage 5V and both output regulator at 3.3V, which full TI part no should I use?
can this be done?
Based on the sample request part no, i did not find one…
Part Number: TLV716P Hello,
I am attempting to model the TLV716P with the following parameters:
Vin: 1.9V
Vout: 1.8V
Iout: 90mA
Here is a snippet of my circuit simulation.
Can you help me receive my desired output?
Thanks
Part Number: TLV716P Other Parts Discussed in Thread: TLV713 , TLV761 Dear Support,
I'm looking for a LDO solution such as our TLV713 ( low cost and small size, 5Vin, 150mAout), but with an output voltage which could be selected (or modified) between…
TLV716P_DPQ_6.bxl
Hi Ed,
There is an issue with the solder paste in the BXL. I am attaching the updated BXL. It should be available on ti.com shortly.
Is this your observation or are you referring to a different problem?
Regards,
Gerold