Part Number: TLV733P
Hello,
I'm using a TVL73333PDQNR device. I would like to ask you about the inrush current at startup. The circuit diagram is shown below. The current is measured at the red circle at startup, but 512mA flows at the peak. It is considered…
Part Number: TLV733P Hi team,
My customer wants to use TLV73312PDBVR for Vin: 1.8V and Vout: 1.2V.
In the datasheet (6.5 Electrical Characteristics), for 1.2V ≤ Vout <1.5V and Iout=300mA, it says that the maximum value of VDO is 420mV.
So, it means…
Part Number: TLV733P-Q1 Hi team,
Could you advise the min max value of TLV73311P-Q1's start time?
It is specified as 250us and I would like to know its min and max especially at Vout=1.1V.
regards,
Part Number: TLV733P
Hi team,
my customer discover large leakage (1mA) at Vin of TLV73315 during "coin battery supply",
as you can see below the red circle, when they decrease the resistor value, the leakage disappear,
also when they use…
Part Number: TLV733P-Q1 Hello Expert, I have question for TLV733P-Q1's AbsMax rating at EN pin. Datasheet explained that it is Vin + 0.3V. However our customer haven't observed any issue even though they are using this device with Vin=1.8V and EN high…
Part Number: TLV733P-Q1 Hi team,
Could you advise how much is the PSRR of TLV73311-Q1 at 1MHz?
I see TLV73318 spec on the datasheet, but I would like to know 1.1V version up to 1MHz.
regards,
Part Number: TLV733P Dear team,
Could you please recommend auto grade sockets could p2p with TLV73311PQDRVRQ1?
Output voltage:1.1V.
Output current:>50mA is fine.
Many thanks.
BR,
Huanfeng.
Part Number: TLV733P-Q1 Hello E2E,
My customer is using TLV73318PQDRVRQ1. They are trying to determine the output impedance of this device. Specifically, here is their question:
"what is the equivalent resistance and inductance of output pins of this…