Part Number: TLV733P
Hi Team,
My customer now evaluate TLV733-Q1 and found that it has quickly discharge function, which include an active pulldown circuit.
But my customer doesn't want this function and do we have another version without quickly…
Part Number: TLV733P Hello E2E,
As the title says, can you tie pins 2 and 5 together to GND? The DS says there no internal connection. Is this acceptable?
Russell
Part Number: TLV733P Hi,
I am planning to use TLV73333PDBVT LDO. As per datasheet Rth JA is 228 c/w. It is also mentioned junction to board thermal resistance is 55.8 c/w. I would like to know what is the preferred copper area i have to provide as my…
Part Number: TLV733P Hi team,
My customer used TLV73333P and they do the testing of "max Capacitive load"(standard 2400uF) and the chip broken when power up.
We guess the broken reason is the output current is too big when power up in Capacitive…
Part Number: TLV733P-Q1 Other Parts Discussed in Thread: LP5907 , Hi Team,
My customer wants to estimate long time drift of output accuracy for 10 years as typ.
Do you have data to estimate such the drift (like Acceleration test, stress test results…
Part Number: TLV733P Other Parts Discussed in Thread: TPS706 Hi team,
The LDO is enabled or disabled when the EN pin is floating? Do we have P2P solutions that EN pin is internally pulled down? Thanks for your support!
Best regards,
Sam Ting
Part Number: TLV733P Hi, team
Is TLV733 P restricted to ambient temperature unless T j exceeds 125 C? Is it safe to use at an ambient temperature of 105 C?
Best Regards,
Hi Sam,
The current limit is specified from 360mA to 700mA. So the current limit will be anywhere in that range, it may not necessarily be right at 360mA.
Improving the inrush will be tricky with those conditions.
The output capacitor is as small…
Part Number: TLV733P-Q1 Hi TI-team
My customer have question.
VEN (HI) [MIN]: 0.9V is recognized as HI if 0.9V or more.
VEN (LO) [MAX]: 0.32V is recognized as LO if it is 0.32V or less.
Is the above recognition correct ?
If correct, what happens…
Part Number: TLV733P Other Parts Discussed in Thread: TLV703 , LP5907 , Hi team,
1. May I know we have good solution can compare TOREX XC6228? since XC6228 standby power just 100nA!!
2. May I know Iq require to standby power?
XC6228.pdf