Part Number: TLV733P Other Parts Discussed in Thread: TLV703 , LP5907 , Hi team,
1. May I know we have good solution can compare TOREX XC6228? since XC6228 standby power just 100nA!!
2. May I know Iq require to standby power?
XC6228.pdf
Part Number: TLV733P Other Parts Discussed in Thread: TPS7A90 Dear Sir,
We are looking LDO that similar with TLV733P, but we need slower rise time > 0.5ms.
Would you help to advice one?
Application:
Vin range : 2~ 3.8V
Iout > 300mA
Vout…
Part Number: TLV733P-Q1 Hi TI-team
My customer want to know the following about thermal information.
1.Do you have the items in this table [RθJA, RθJC(top), RθJB, ψJT, ψJB, RθJC(bot)] shown in the image diagram ?
2.What is the difference between…
Part Number: TLV733P-Q1 Hi Team,
Whether TLV73312PQDBVRQ1 could work normally in the following application?
Vin 5V
Vout 1.2V
Iout 200mA
Temp -40-85℃
Power=(5-1.2)*0.2=0.76W
0.76W*198.3=150℃>125℃. It is too high...How could it work normally…
Part Number: TLV733P Hello,
I have a question about the LDO can it be used to run a mechanical switch button to operate at a regulated voltage level?
The reason being is that I have a limited space (2mm x 2mm) and one of the PIO require voltage…
Part Number: TLV733P Hello,
We are using TLV733P on our board. But the problem with TLV733P is the maximum input voltage is 5.5. So i need a drop in replacement for TLV733P which has all specifications same as TLV733P but with higher input range.…
Part Number: TLV733P-Q1 Hi,
I am considering using the TLV73333PQDRVRQ1 device. (Question) Is the overcurrent protection (ILIM, IOS) and thermal shutdown (TSD) described in the data sheet electrical characteristics 100% tested? Or is it a sampling inspection…
Part Number: TLV733P-Q1 Hi TI-team
My customer wants a foldback waveform.
Can you get the waveform when Vout = 1.2V in the graph below ?
Best Regards,
Koji Hayashi