Part Number: TLV751 Hello,
My customer is interesting the dual LDO, but concerning thermal performance due to its higher density.
Do you have comparison data of thermal between single and dual of TLV751?
Best regards,
Katsu
Part Number: TLV751-EVM Hi Team, Our customer is requesting the board dimension of TLV751-EVM. Can you share its dimension so I can inform the customer? Thanks! Jonathan
Hi Albert,
The pin out in the recommended layout is correct in Figure 44. The one in the pin configuration page is wrong. We are fixing this error and the updated datasheet should be online in the next week or two.
We apologize the inconvinence…
Hi Falguni,
This will probably be the best one: https://www.ti.com/product/TLV751/part-details/TLV751180330PDSQR
Dual output fixed 1.8 and 3.3 with 500mA load regulation. Noise performance is also plenty good enough.
Best regards, Jeff McPherso…
Part Number: LP3996 Other Parts Discussed in Thread: TLV751 Dear Sir,
Instead of LDO: LP3996_1, we are looking for an alternative part for a buck converter with a Power-On Reset function. (If current ratings are a little different then also please suggest…
Hi Wei,
If automotive grade is not a hard requirement, TLV759P is a low cost alternative to TPS7A52-Q1, TPS7A91 is a good low cost & low noise alternative to TLV751 device. TPS7B91 is a low cost alternative to TPS7B69-Q1. Thanks!
Regards,
Srika…
The LDO should be able to output 1.8V and 2.9V(2.85V). For TLV751, the P/N seems to be TLV751180290(TLV751180285). But I can not find them anywhere.
This is a space senstive project. Dual output LDO with fixed version is best choice.
Part Number: LP5912 Other Parts Discussed in Thread: TLV751 , TPS7A87 Hi
We are looking to upgrade the max current of the LDO we are using (the LP5907QMFX-3.3Q1 with max 250 mA) with a new one with more current (for example the LP5912).
Is there a…