Part Number: TLV757P Other Parts Discussed in Thread: TPS737 Hi, support team
My customer need a replacement of TLV75733PDRVR.(PIN to PIN) TLV75733PDRVR is found, but TLV75733PDRVR's Pin2 is NR when use in Fixed voltage. Datasheet write "connecting…
Part Number: TLV757P Hi,
According to Figure14 on the TLV757P datasheet P.9, we can find the Dropout voltage graph "2.2-V Dropout Voltage vs Iout". Which is correct condition on this graph, VIN=3.3V or VOUT=3.3V? Please let us know.
Also, my…
Part Number: TLV757P Other Parts Discussed in Thread: TPS7A37 , TLV759P , TPS746
Hi team,
Is there a development plan to release TLV757P with 0.95Vout option?
If there is no plan, I will suggest TPS7A37 or TLV759P to customer for 1A power rail.
Regards…
Part Number: TLV757P Hi Team,
According to Data sheet, accuracy of TLV7530PDRVR will be ∓1%.
Customers now require ±1%
Is there any concern such as temperature dependence?
Best Regards,
Maki
Part Number: TLV757P Other Parts Discussed in Thread: TLV755P Dear all,
I am looking for voltage regulator with following requirement. Vin 5V, Vout 4V and Vout 3.3V.
My Application is to supply and DC bias for RF amplifier.
I came across TLV757P and found…
Part Number: TLV757P Hello.
There is a problem when EN pin voltage is higher than IN voltage.
Briefly describing my system, VIN is lipo battery(3.0~4.2V), VEN is connected to Vbatt(3.0~4.2V) or external usb power(about 5.0V).
TLV75733 works well usually…
Part Number: TLV757P Hi TI,
We use the SOT-23 package, our customer ask us , what's parameter do we use for calculation the thermal temperature?
If we measure the IC surface, what parameter do you suggest to calculate the junction temperature? Rjc…
Part Number: TLV757P Other Parts Discussed in Thread: TINA-TI Hello,
I am attempting to create a TINA-TI model for the TLV75712P.
When I was attempting to add a new macro model in TINA-TI I received this error:
Redeclaration of identifier: D_D1.Line#2…
Part Number: TLV757P Tool/software: WEBENCH® Design Tools I do not find a design for the provided Part number. Please help out on this. I do not even get LtSpice model/TINA model of the above mentioned part.
Part Number: TLV757P Hello team!
Could you please tell me the current protection behavior about the device?
I read 7.3.3 on DS but not sure my understanding is correct or not.
For the short event, the current is limited by 755mA(typ).
For the overcurrent…