Part Number: TLV759P Hi TI Team,
Please clarify the pin 5 of TLV759P with the description "DNC' (Do Not Connect) means.
There is wire connected internally on pin 5. I'm not sure if DNC also means no connection.
Kindly advise.
Thanks!
Part Number: TLV759P Dear Specialists, Customer is considering a Li-ion cap charge control circuit using TLV759P. And trying to realize a current limiting function of 300mA with an additional circuit. They wants the schematic check information by TI.…
Part Number: TLV759P Hi,
I am considering using a TLV75901PDRV device, but I would like to ask you about the sequencing of this device. Although VIN=5.1V and VOUT=4.8V are set, the EN signal (1.8V is applied) is applied before 5.1V is supplied. Is there…
Part Number: TLV759P Hi, Could you tell me about the thermal information data acquisition conditions? Please tell me the board area and PCB information when this data was obtained. Customers want to compare their information with their own board size…
Part Number: TLV759P Hi,
I asked a question in the following thread about setting the device constant of TLV759 before. With that advice in mind, I came up with the following constants: Is it OK to use this constant?
VOUT: 4.9V R1 = 174kΩ, R2 = 22kΩ…
Part Number: TLV759P Hi,
What are the recommended constants for R1, R2, and Cff when setting the output voltage to 4.9V or 4.3V? Looking at the datasheet, it seems that PSRR improves with Cff, so I would like to use Cff.
Best regards,
Part Number: TLV759P Other Parts Discussed in Thread: TLV757P , TLV755P Hi TI team,
My customer request temperature characteristics data of LDO.
Do you have any data on temperature characteristics in addition to the datasheet?
We need Icl (Output…
Part Number: TLV759P Hello,
My customer is considering about Vdo of TLV759P.
Their requirements are as follows.
Vin : 1.8V
Vout : 1.35V
Iout : 0.6A (max)
It is written In datasheets as follows. Vdo = 580mV(max) 1.2 V ≤ VOUT < 1.5 V @ 1A…
Part Number: TLV759P Other Parts Discussed in Thread: TPS7A91 Dear Sir/Madam
I'm searching for an LDO with more than 85%efficiency for converting 5V to 3.3V and 3.3V to 1.2V at 1A.
When I referred TLV759P I found that it suits my requirement. But…
Part Number: TLV759P Hello,
This device has internal soft-start. Is it “constant current operation” during startup with soft-start?
thanks and best regards, Katsu M