Part Number: TLV760 I have a switching regulator ( LMQ61460AAS, 24V Input) with a variable output voltage (22V - 10V) and also need a fixed voltage of 3.3V (max 8mA). I chose the TLV760-33 for the 3.3V.
Currently I have connected the linear regulator…
Part Number: TLV760 Hi,
Could you please make the graph of Psi-JT vs " PCB copper coverage are such as Vdd/GND Size"?
The result of thermal on Package top is different from calculation with Psi-JT. My customer is thinking Thermal pad size such as…
Part Number: TLV760 Can customer use TLV76012DBZR(SOT-23 package) as wave soldering assembly ?
If yes , Do you have any temperature profile for wave soldering documents ?
Best Regards
Koji Sakurai
Part Number: TLV760 Other Parts Discussed in Thread: TLV767 Hi team,
My customer use TLV76050DBZT to translate 17V to 5V, and 5V just power for 1pcs AMC1305. Below is their SCH.
But at sometimes, TLV760 output shutdown 1ms and then recover. We test…
Part Number: TLV760 Hi Team,
My customer is now considering TLV76015DBZR and he wants "Output Voltage vs Input Voltage" graph for TLV76015.
There is only graph for 3.3V and 5V output in p.7 of TLV760 datasheet.
And please kindly also provide other…
Part Number: TLV760 Other Parts Discussed in Thread: TPS7B69 , TPS709 Hi all,
I am looking for a replacement for the LM3480IM-15NOPB, where I have found the TLV76015DB. Can you help assist me in determining differences between the two parts?
www…
Part Number: TLV760 Hi team,
I would like to confirm about Figure 16 "Output Current vs Input Voltage".
It indicates "Vout(Red)=3.3V".
Is it correct to think that Red line shows max output current with various Vin condition from 5.8V to 25.7V under…
Part Number: TLV760 Hello team,
What happens when the 5V voltage input at output pin in case of no voltage at VIN pin.
Does TLV76050 have internal clamp circuit at VOUT pin ? If yes, the customer can avoid any issues by putting current limit resistor…
Part Number: TLV760
Hi,
I am using TLV76033DBZR for to convert 5V to 3.3V.
I am plan to use both input and output capacitors are 0.1UF(Y5V)Caps
In TLV76033DBZR datasheet it shows input need greater than 0.1uF.Also TI suggest for to " Use C0G,…
Part Number: TLV760 Hi,
Please let me know the ripple value of TLV76033DBZR.
Also please let me know the output voltage tolerance of LM5010AMHX/NOPB.
Warm regards,
Monisha OM