Part Number: LP3891 Other Parts Discussed in Thread: TLV767 , TLV761 , LP38502-ADJ Tool/software: Hi Mr./Mis,
Is there any risk in using the LP3891 instead of the Richtek DS9183? https://www.richtek.com/assets/product_file/RT9183/DS9183-24.pdf
Part Number: TLV1171 Other Parts Discussed in Thread: TLV761 , TLV1117 , , TLV757P Hi team:
pls advice the P2P next Gen of TLV117112DCYR, i see the TLV761 is the next GEN, but no 1.2V output version yet. can you help to update this ?
Part Number: UCC28881 Other Parts Discussed in Thread: UCC28911 , UCC28910 , TLV767 , TLV761 Hi team,
Does UCC28881 support 7V output with 200mA~300mA load in non-iso flybuck topology? As read from datasheet, the limitation is 225mA in open frame…
Hi Wei,
Apologies for the delay in getting back to you, I was out of office through last week. I do not see any concern with using TLV1117LV (apart from the noise spec). From a supply continuity point of view, I would urge you to consider TLV761 instead…
HI Sukrat,
For most LDO's the bandwidth of the error-amplifier is less than 100Khz. So when we simulate for stability for modern LDO's, we are using the minimum ESR typically around 10-20mOhm.
The 0.2-10 Ohm range you mention seems to be referring…
Hi Wei,
We would not recommend operating with a 6V nominal input voltage, if the input voltage never exceeded 6V you MAY be ok. However, if there are any deviations coming from the upstream switching regulator that would put you at significant risk…
I have posted a message here:
https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/1341543/tlv761-supplying-appropriate-voltages-from-5v-fpga-for-ddc232/5110230#5110230
However, an important part of this is understanding…
Hi TISL,
Unfortunately, the TLV761 has active pulldowns on both outputs. So if one is disabled it tries to pull down the rail.
We do have the TPS780 which has a pin selectable output but I only see a 3V/1.8V version released. We do not have a…
Other Parts Discussed in Thread: TLV761 Hi, I would like to know the number of years before the obsoletency of this product. : LM1117MP-ADJ Thanks in advance, Emeric