Part Number: TLV766-Q1 Hello team
I received question from cutomer
Question1
In the 6.4 Theemental Information bullet of the data sheet, Each one has a defined thermal resistance, but is this value the typ value or the max value?
Question2
What is the…
Part Number: TLV766-Q1
Hi team,
I would like to control the Vout (set to 0.9V) start up time between 150us to 3ms from VIN=3.3V.
This device has typical 500us soft start.
Could you advise if this device can meet my requirement over PVT?
regards,
Part Number: TLV766-Q1 Other Parts Discussed in Thread: LM317 , Hi Team,
Our customer would like to confirm if they can use the TLV766-Q1 as a constant current driver like LM317. Aside from the Output Pulldown function, the internal configuration of the TLV766…
Part Number: TLV766-Q1 Other Parts Discussed in Thread: TLV767-Q1 , , TLV767 Hello,
from Figure 7-2 in the datasheet I have a doubt about the match between the available output voltages (1.2, 1.8, 3.3, 5.0) and the values/ranges of R1 and R2.
It seems…
Part Number: TLV766-Q1 Hello Team,
Our customer have some question about line regulation spec. It shows the max is 0.02%/V.
Q1. Does the line regulation characteristic of TLV766-Q1 will increase monotonic? (If Vin will increase, Vout will increase as…
Part Number: TLV766-Q1 Hi!
I would like to know if there need to be additional parts (Schottky diode?) if we expect that a secondary supply may apply voltage to OUT/SNS.
For example: 1] The TLV766 may have 12V IN with a fixed output of 3.3V. 2] The 12V…
Part Number: TLV766-Q1 Hi team,
Customer report there is a output abnormal issue with BCI test.
The current injection clamp as shown in below picture's circle that inject interference signals of 1-400MHz, and then there will be AC signal in this section…
Part Number: TLV766-Q1 Hello Team,
Our customer plan to use TLV76601QWDRBRQ1.
I think the EN pin has internal pull-up resistor. Can you please let me know the min/typ/max of the pull up resistance?
Thanks,
Yuta Kurimoto
Part Number: TLV766-Q1 Hello Team,
I have a question about Dropout voltage(Vdo)
I understand if the input voltage is low, the Vout also decrease based on the equation Vdo=Vin-Vout.
In this situation, is there any other disadvantage such as noise, power…
Part Number: TLV766-Q1 Hello Team,
Thanks for your support.
Our customer want to use TLV766-Q1 adjustable output version. They request Output voltage noise(Vn) data in order to choose the device. Can you please provide the data?
Parameter : Output voltage…