Part Number: TLV767 Hi,
I am simulating the TLV767 model in PSPICE. when I grab the model from the built in TI library, I actually am given the model for the TPS74601. What's going on?
Thanks,
Ethan
Part Number: TLV767 Hello,
Here is a little confusing. In the datasheet 6.5 EC table, the accuracy of VOUT is +/-1% over temp. The question is that is VREF accuracy +/-1% included in the VOUT accuracy?
Is the feedback resistor tolerance taken into account…
Part Number: TLV767 Dear Team,
I am using TLV76733DGNR in my design
I/P = 5V (Coming from a switcher)
OP = 3.3V,1A
My schematic is given below. May I know your comments.
Regards
HARI
Part Number: TLV767 Other Parts Discussed in Thread: TPS62170 , How is the variation of the VREF over the temp range?
In the E/C table, it only specify the 0.8V,typ value. Thanks.
Regards
Brian
Part Number: TLV767 Hallo everyone,
I made a custom PCB for the ESP32 and choose the TLV76733DRVR as a LDO Voltage Regulator, I've put the Cin as 1 Micro Farad like what is written in the Datasheet and the Cout as 2,2 Micro Farad, and yet got an Output…
Hi Ethan,
Unfortunately the LTSpice license agreement legally prevents TI from assisting you in any way with models in LTSpice. You may download a free copy of PSpice for TI and run these simulations in that software if you would like. We can offer further…
Part Number: TLV767 Other Parts Discussed in Thread: TPS7A47 Hi team,
I'm looking for a low cost device with following requirements.
Soft-start function
Vin_min: 4.5V
Vin_max: >21V(Higher than 35V would be more ideal)
Vout: 3.3V
Iout: 0.5A
My…
Part Number: TLV767-Q1 Hi,
I am putting this device to power CAN transceivers on my PCB. The supply to the device will be constant and I would need to enable the device when leaving sleep mode on my PCB through the enable pin. As this device is on by…