Part Number: TLV9002 Other Parts Discussed in Thread: TLV9004 TINA_TLV9002_SIM.pptx TLV9002_SIM.TSC Hi, TI team.
I use your TLV9004 opamp. I'm just changed resistor value (R3 , refer to the attached file) and opamp output voltage is changed. but there is…
Part Number: TLV9002 Hi
Im having trouble when following the design steps (page 2 of the application note, or page 262 of Analog Engineer’s Circuit Cookbook: Amplifiers Second Edition SLYY137 - 03/2019).
Where is this equation come from?
I kn…
Part Number: TLV9002 Other Parts Discussed in Thread: TLV9062 , TINA-TI Hi all Would you mind if we ask TLV9002 and TLV9062? Comared with TLV9062, TLV9002 is less than input voltage noise despite of big input noise density. We assume that input voltage noise…
Part Number: TLV9002 Other Parts Discussed in Thread: TINA-TI Where can I get the SBOMAV6.zip SPICE Simulation File for this Temperature sensing with NTC circuit?
Part Number: TLV9002 Other Parts Discussed in Thread: UA741 Dear team
May I ask about the sboa275a? http://www.ti.com/lit/an/sboa275a/sboa275a.pdf
Instead of using TLV9002, I used UA741 for the experiment.
When supplying +15/-15V power and 1kHz square…
Part Number: CC3220MOD Other Parts Discussed in Thread: TLV9002
Hi,
We are Using CC3220MODSF12MOBR CONTROLLER with TLV9002 OPAMP to read the CT Voltage.
We are using Voltage based CT (20A/1V), After connecting to the Line-Load, It showing 0.115VAC by…
The LM2904 does not have rail-to-rail inputs or outputs. With a 3.3 V supply, it is not guaranteed to handle voltages above 1.3 V.
The LM358LV/LM321LV would be able to handle up to 2.3 V. The TLV9002/TLV9001 has rail-to-rail I/Os.
Part Number: TLV9002 Hi team.
I'd like to know about the Vout vs slew rate.
Our situation is when the output voltage is decrease and the slew rate decreases.
Sincerely.
Kengo.
Part Number: TLV9002 Other Parts Discussed in Thread: TINA-TI Hi team,
My custom needs SPICE Simulation File SBOMAV6 in the link below. Could you help find it?
Best Regards,
Amy