Part Number: TLV9151 Other Parts Discussed in Thread: TLV9161 , , TLV9152 Tool/software: Hello,
For TLV9151 and TLV9161, when i try to use the PSpice model I get the following error:
ERROR(ORPSIM-15108): Subcircuit TLV9152 used by X_U1 is undefined…
Part Number: TLV9151 hi
is there any reference document that explains rectification effect in OP AMP ?
is there any test setup recommended to measure it ?
thx
eli
Part Number: TLV9151 Hi,
From the datasheet as shown below, does the highlighted statement means that the signal input pins are allowed to exceed (V+)+0.5V if the current is <10mA?
In my design, the supply voltage to TLV9151 is 5V. However, we…
Hi Katherine,
You can consider the TLV9151 in this case, which is a 4.5MHz, 16V, single channel, low Vos and low noise amplifier. It’s RRIO and we also have the dual and quad channel available online if needed.
Here is a table showing the performance…
Part Number: TLV9151 Other Parts Discussed in Thread: TLV9152 Is there a TINA or PSPICE for TI model available or in the works?
Thanks,
Joe Stephan
TI FAE
Part Number: TLV9151 Other Parts Discussed in Thread: TLV2370 , , TLV9051 , OPA863 , OPA734 Hi,
on product page of TLV2370 there is a note that TLV9151 ist drop in replacement (pin to pin upgrade). But to enable TLV2370 the shutdown pin must be pulled…
Part Number: TLV9154 Hi, in the latest (rev.D) datasheet of TLV915x there is some inconsistency in regards to EMIRR - there are two plots of EMIRR vs frequency and they differ significantly. One is Fig. 6-41 and the other Fig. 7-1. There are differences…
Part Number: TLV271 Other Parts Discussed in Thread: TLV9151 Hi,
I have a TINA simulation of the TLV271 in a differential amplifier configuration. The simulation worked well however the actual circuit does not. It appears that the simulation generates…
Part Number: SN54F241 Other Parts Discussed in Thread: DAC081C081 , BUF634A , TMUX1219 , LMH6321 , TLV9151 Tool/software: Hello,
We are looking for a component that can increase the driving capacity of digital I/O from an FPGA.
Additionally, we need…