Part Number: TLVH431 Other Parts Discussed in Thread: TPS3762 Tool/software: Hello,
can you please help me to classify the TLVH431 device according the SN 29500 standard? I have to perform an FMEDA analysis with the tool Silcal and the classification…
Part Number: TLVH431 Our circuit causes a condition where when the part regulates it clamps from 9.3V to 4.3V in 1msec with a peak current of 250mA for 1msec. This instaneous power is a triangle wave with the voltage across the part 9.3 to 4.4V and the…
Part Number: TLVH431B Other Parts Discussed in Thread: TLVH431 , Why did the circuit work properly after removing C28? Given that the current is not high, why would adding capacitor C28 cause a low-voltage issue, and why did removing it resolve the problem…
Part Number: TLVH431A Other Parts Discussed in Thread: TLVH431 , TLV803E , TL431 Hello,
In the TLVH431 datasheet, under chapter 8.2. Typical Applications, it is mentioned that the TLVH431's output low level voltage in open-loop/comparator mode is ~1V…
Part Number: TLVH431 Tool/software: Hello,
I think there is a problem with my design method. Please give me some advice.
[About the assignment]
We are considering using the TLVH431AQDCKR for output control of a flyback converter.
The circuit…
Part Number: TLVH431 Other Parts Discussed in Thread: LMV431 Hi
(TLVH431 vs. LMV4312) models, except for different temperatures, Are there any other differences? Are they interchangeable (temperature factor is not considered!)?
Part Number: TLVH431 Other Parts Discussed in Thread: LMV431 , , LM431 I am doing a bench test comparison of the TLVH431CLPR versus LMV431 voltage shunt devices.
The component test using the circuit below resulted in Vref = 1.24v and Vout = 2.5v as…
Part Number: TLVH431 Hi,
Customer know the capacitor from CATHOD to GND (output capacitor) will affect the stability. And I see no capacitor is needed for VREF to GND, but customer want to know if the parasitic capacitor of the board from VREF to GND…
Part Number: TLVH431 Other Parts Discussed in Thread: TL431 , ATL431 Hi team,
The datasheet states "TI recommends to choose capacitors that will give a phase margin > 5° to guarantee stability of the TLVH431” I think phase margin around 5° should…