Part Number: TLVH431 Other Parts Discussed in Thread: TLV431 Hi Team,
I find the schematic showing as below, and the Cload recommended value is 0.1uF
I'm not sure relationship between CL and PM. I see when Cload = 0.1uF, the PM~0degree
So when we…
Part Number: TLVH431 Hi team,
My customer is using AM572X EVM and found the TLVH431 in #5 page as attachment, could you please help to show how this circuit work and why we need this circuit?
Thanks.
ARM MPU AM572X Industrial EVM.pdf
Part Number: TLVH431 Other Parts Discussed in Thread: TINA-TI , TLV431 , , LMV431 Tool/software: TINA-TI or Spice Models Hi,
several weeks ago in February I reported some problems with the SPICE models of the shunt regulators TLVH431, TLV431 and LMV431. …
Part Number: TLVH431 Hi Team:
Could you help to provide wave soldering data of TLVH431 (1V24 1mA to 100mA 1% SOT-23) for customer request ?
Thanks.
Regards / Mark
Part Number: TLV431 Other Parts Discussed in Thread: TLVH431 , LMV431 hello everyone,
I use the following design from SLVA987A with a TLV431:
I have the following issue, this circuit work very well with TLVH431 but not TLV431.
When the Vref voltage…
Part Number: TLVH431 Other Parts Discussed in Thread: TLV431 , TL431LI Hello,
I am using the TLVH431 simulation model in LTspice to evaluate the pulse response specified in datasheet, fig 12 and 13 on page 11 and 12. Despite I use the same circuit as in…
Hello Barry,
Unfortunately we do not test for this spec on this device. You can consider using the TLVH431 . It is a similar part and includes an off state current spec.
I also do not think this circuit will work correctly. The cathode of the shunt regulator…
Hello Charlie,
We do not have a device with a fixed output of 2.2V but you can use an adjustable device such as TLVH431 to set the output to 2.2V.
You can use this circuit and select R1 and R2 to get 2.2V
Thanks,
Walter
Hi Joshua
1、the voltage of cathode-gnd is 0.86V. the voltage of Vref-gnd is 1.34V.
2、Our application scenario is open loop of TLVH431,We want to know the "voltage - current - temperature relationship" of the TLVH431 when the open loop "low" mode…