Part Number: TLVH431B I use the below formula to calculate
Vout = (1+R1/R2) x Vref
= (1+105/K127K) x 1.25V
= 2.28V
But TINA simulation does not show the same with calculation.
it shows Vout = 1.25
Hello Suja,
The closest alternative would be the TLVH431 series which has a rating of 18V vs 30V on LMV431. Hope this works.
https://www.ti.com/lit/ds/symlink/tlvh431.pdf
TLVH431B | Buy TI Parts | TI.com
Thanks.
Hello,
Please refer to the functional safety information of TLVH431B-Q1. See attached. The team has informed me this information applies to TLV431B-DBZQ1.
Regards,
Oscar Ambriz
TLV431B-Q1_FS_Information.pdf
Other Parts Discussed in Thread: TLVH431B Dear, All
A customer wants to know the variation tendency of Reference voltage of TLVH431B. Then, it is a question. Is Reference voltage of TLVH431B sorting out? Or didn't it sort out? Or is voltage adjustment…
Part Number: TLV431B-Q1 Other Parts Discussed in Thread: TLVH431B-Q1 , Hi There,
I appreciate the recommended operating voltage max is 6V for the Cathode Voltage in this part, but would there be instability if the part was set to a typical voltage of 6…
Part Number: LMV431A Other Parts Discussed in Thread: LMV431 , TLV431 , TLVH431B , TLVH431 Hi sir:
I can’t find minimum working cathode voltage when ref>1.5v in datasheet;
can someone help me? i want to use it as a comparator ;
sean
Other Parts Discussed in Thread: TLVH431B Dear Sir,
I'm using the part TLVH431BIDBZR in my design.
In the datasheet, the reference voltage Vref is provided for TA=25 degC.
I would like to know the Vref range for the ambient temperature of +55 degC…
Part Number: TLVH431A-Q1 Other Parts Discussed in Thread: TLVH431 Hi Team,
We are using TLVH431AQDBVRQ1 in a ADAS project for 3.3V rail overvoltage detection and shut down. The overvoltage threshold is set as 4V typical. The schematic is shown as below,…