Part Number: TLVM14406 Tool/software: How about a footprint and symbol for this device?
Would certainly help to use it.
Since there is an EVM for the thing, I assume there's a footprint running around somewhere?
Part Number: TLVM14406 Tool/software: Looking at page 36 of the datasheet, table 8-4 lists materials for the sample application circuit 2.
Input capacitors Cin1,Cin2 are listed as 4 2.2uf capacitors.
Same page, 4 paragraphs down
Paragraph 8.2…
Part Number: TLVM14406 Tool/software: Hi team,
I have two questions.
First, I believe it is possible to adjust the soft-start time with an external capacitor. Could you please provide the specific formula for determining the rise time?
Secondly…
Part Number: TLVM14406 Other Parts Discussed in Thread: TPSM64406 Tool/software: The TLVM14406 page states the following.
Create a custom design using the TLVM1440x with the WEBENCH Power Designer However, the model number does not match.Please tell…
Part Number: TLVM14406 Tool/software: Hi
We see the VOUT2 stays close to the generated value (1.8V) even after the EN2 is low.
Attached the schematic snippet & waveform for better understanding
Both EN1 & EN2 are shorted and driven by the FPGA-…
Part Number: TLVM14406 Other Parts Discussed in Thread: TLVM14404 , TLVM13620 , TPSM33625 , TPSM63602 , TPSM64406EVM , TPSM64406 Tool/software: Dear Specialists,
My customer is considering TLVM14406 and TLVM14404, they have questions.
I would be grateful…
Part Number: TPSM64406 Other Parts Discussed in Thread: TLVM14406 Hi team,
The TPSM64406 datasheet states that the device can be used to generate a negative output voltage. In this context, is it possible to configure only one of the two outputs as…
Part Number: TPSM64406E Other Parts Discussed in Thread: TLVM14406 Tool/software: Hello,
This is a call for DC/DC suggestions.
The crucial issue here is extremely low radiated and conducted emissions.
As for output ripple, we could always add an…
Part Number: LM62460 Other Parts Discussed in Thread: LMR66430 , TLVM14406 , TLVM23625 Tool/software: Hello team,
I'm creating the design with the condition, Vin:24V / Vout: 2.3V / Iout :2A.
If I use LM62460, Webench is warning about minimum On time…