Part Number: TM4C1231H6PM Other Parts Discussed in Thread: CCSTUDIO Tool/software: Code Composer Studio I'm getting errors in Run/Debug Settings and breakpoints have stopped working. This has been working fine in the past. If I select "Edit..." for…
Part Number: TM4C1231H6PM
Hello,
I am hoping to get some clarification on using a Timer based PWM output to control a couple cathodes of a tri-color common anode LED. I setup the pins to be gpio outputs od (open drain) with GPIOPinTypeGPIOOutputOD followed…
Part Number: TM4C1231H6PZ Other Parts Discussed in Thread: TM4C1231H6PM Tool/software: Code Composer Studio Hi all, I have a project targeting tm4c1231h6pm processor, the debugger works fine and it stops at the main () after it is launched. However when…
Part Number: TM4C1231H6PM Other Parts Discussed in Thread: SEGGER , TM4C1290NCPDT Tool/software: Code Composer Studio I had been using Code Sourcery (Codebench) and have moved my sources to CCS (8.3.1.00004). I'm using code that has been running with the…
Part Number: TM4C1231H6PM
Hi,
My system is running with FreeRTOS, it has interrupts and the system clock is 50MHz.
For this errata's requirement,
what does it mean by "Interrupt must be disabled" ?
Also, I would like to try to reproduce…
Part Number: TM4C1231H6PM
Hi,
I have a system that uses PLL during run mode and disables PLL before going into deep sleep. Do I have to put a small delay after calling SysCtlClockSet() for the setting to take effect? If so, what is the recommended time…
Part Number: TM4C1231H6PM Hello,
The RTC of TM4C1231 can't be saved When power up again during we test board function . About 30% failure rate for this. Would you please give your advice on this? thanks.
Part Number: TM4C1231H6PM
Hi All,
I have a system that samples data from some sensors and then goes into deep sleep mode. The way that the system gets waked up from deep sleep is through a GPIO interrupt from an outside source. There are multiple GPIO…
Part Number: TM4C1231H6PM Other Parts Discussed in Thread: TM4C123GH6PM I have a GPIOF_Handler function. Inside this function, i need to know if a sw1(PF4) is pressed or if a sw2(PF0) is pressed, and then, execute a code properly. How i do this without…