Part Number: TM4C1231H6PZ Hi team,
We are using the TM4C1231H6PZ in our application and are wondering if there is a way to permanently lock the EEPROM. I see that there are the EEPASSn registers to lock it but if an intruder knows the password, then the…
Part Number: TM4C1231H6PZ Wondering what the breakdown is for naming the TM4C123 1 H6PZI7R?
Also, is there an EEPROM failure for the rev 6 version of this board? Similar to what was found on the TM4C123 G H6PZI/TM4C123GH6PZI6R.
By failure: (Copied from another…
Hello Harry,
As Charles stated, this is being handled offline now, and he has communicated with you via email on this topic. At this point, the topic is simply not fit to discuss on the public E2E forums which is why we are saying we need to close this…
Part Number: TM4C1231H6PZ dear all,
when i use TM4C1231H6PZI MCU with frequently data write in EEPROM, it will break down after a long time write. do i need some reset operate?
In my application, we made about 500 boards and ran after half year customer…
Part Number: TM4C1231H6PZ Hi team,
Do we have any information about Single Event Upset (SEU) handling (detection/correction/notification) on the TM4C1231H6PZ? Is this feature supported on this class of devices? If not, do we have any MCUs that feature SEU…
Part Number: TM4C1231H6PZ
I am trying to implement the same sequence of steps with different parameter values except I did not invert. The output is doing nothing. I can monitor the registers and TIMER_TAR is changing as expected. Is it possible that…
Part Number: TM4C1231H6PZ
Hi team,
We are looking to use the TM4C1231H6PZ in our design. We are looking at the boot_usb example and in the bl_crc32.c file at the CheckImageCRC32 function. Based on the definition of CLASS_IS_TM4C129, it appears this will…
Part Number: TM4C1231H6PZ Question from customer:
I have a question regarding the TM4C1231H6PZ that we're thinking of using for our internal-use evaluation board. (This is to test an internally developed ASIC).
The ASIC will have a SPI interface…
Part Number: TM4C1231H6PZ
I'm sorry i'm forced to ask questions here and not solve this problem on my own, but i'm positively stuck at the dead end.
Here is the problem: after some time trying to comprehend manual and playing around with…
Part Number: TM4C1231H6PZ Hi Support,
I would need your help regarding RTC time trimming.
Is a possibility to output LFOSC clock 32768Hz on a pin to measure frequency accurate? (Measurement directly on XTAL OSC pins would influenced frequency).
Can you…