Part Number: TM4C123BH6PZ Do you know the difference between TM4C123BH6PZI And TM4C123BH6PZI7R ?
Normally there is just a “R” for TR but I’m not sure what the “7” denotes.
We have the 7R in stock I wanted to offer as alternate…
Part Number: TM4C123BH6PZ Hello,
I'm attempting to reset a bricked chip using the dbgjtag.exe utility.
The instructions state that the utility package must be "6.0.83.0 or latest".
My version is "6.0.628.3" which is older than the required…
Part Number: TM4C123BH6PZ Hello,
First of all let me explain that I have seen a few posts similar to this issue already. I still have some questions regarding what is happening in my system and the origins of the problem.
I am using the TM4C123BH6PZ in…
Part Number: TM4C123BH6PZ Other Parts Discussed in Thread: TM4C1294NCZAD
Tool/software: Code Composer Studio
Hey Bob, I was working on a project involving sampling external analog signal. I saw your post above in which you provided with a example file…
Part Number: TM4C123BH6PZ In developing for the TM4C I am using the SSI peripheral with the following settings: Freescale SPI with SPO=0 and SPH=0. With these settings the SSInFSS is toggled between each word of information on a continuous transfer. In…
Part Number: TM4C123BH6PZ Other Parts Discussed in Thread: UNIFLASH Tool/software: Code Composer Studio In setting up the scenario the specified controller is used on a custom board. The debugger is a Blackhawk USB-560M (cTI 20-pin header). Utilizing CCS…
That was the issue all along. It is interesting as this breaks from the Tiva implementation of the number 1 refers to module 1 just like SSI1 or UART1. Thanks for getting to the root of the problem as it functions now as expected.
Tim
Part Number: TM4C123BH6PZ Question:
I see this processor can run with its own internal oscillator.. does that run at the max speed of the part.. or??
From what I can tell from the datasheet - the maximum self-clocking speed is 16MHz (please confirm…
Part Number: TM4C123BH6PZ The project I'm on is a resurrection of a project from a different company. I've pieced together the tool chain and am at the last stages (I hope). I'm trying to create a bin file but have not been successful.
I have…
Part Number: TM4C123BH6PZ Tool/software: TI-RTOS The project I'm on is a resurrection of a project from a different company. I've pieced together the tool chain, but have not been able to get it to work. I get the following error message.
Buildfile…