Part Number: TM4C123BH6ZRB Hello
In the data sheet, it mentions that the Rs is Max at 500ohms and Radc is max at 2.5Kohms.
What does these two parameters mean? how do they impact customer's design to get a better ADC accuray?
Thanks
Yihe
Part Number: TM4C123BH6ZRB Hello Team
I download the TIVA software package and the bootloader folder contains the source codes. but it does not includes CCS project files like other examples in the package. Where can I get it?
My purpose is to compile the…
Part Number: TM4C123BH6ZRB Dear TI Team.
we see some different behaviors between two DAte Codes, can you please check if there is something known
Some of the new Versions will get destroyed while programming via JTAG, please advise
Part Number: TM4C123BH6ZRB Hello
In the TM4C123BH6ZRB, it mentions that a copy buffer. the copy buffer is only used when a main block is full. My question is how big is the copy buffer? how can a application know that the copy buffer is full?
In the EEPROM…
Part Number: TM4C123BH6ZRB Hi Charles,
sorry for related answer.
Now I tried the unlock by using your proposed TM4C123 lounchpad and your attached maual.
First it didn't work because of low reset Signal (2V instead of 3V3).
After handling the reset…
Part Number: TM4C123BH6ZRB
Hello Team
Our customer is asking for the Vil/Vih and Vol/Voh specifications for the I2C interface ?
In the data sheet Table 23-6, it lists the Vih/Vil, Vol/Voh for the GPIO pad. Is this also applied on the I2C or I2C have its own…
Part Number: TM4C123BH6ZRB Hi
My customer wants to know that the GPIO impedance(under Hi-Z) mode when device is reset. The reason is that the IO is used to control a gate of FET and engineer wants to the gate voltage probably below 400-500mV when device…
Part Number: TM4C123BH6ZRB Hi, the sampling rate on the TM4C123BH6ZRB is 1 million samples/second. Can the sampling rate be configured or slowed down?
Thanks!
Part Number: TM4C123BH6ZRB Hi,
I recovered a locked TIVA microcontroller via debug port unlock sequence (by I-Jet Trace in IAR Workbench for ARM)
(s. Manual p. 199: Performing a total of ten JTAG-to_SWD and SWD-to-JTAG swith sequences while holding the…
Hi Jorgen,
As you are aware, the ZRB package is being EOL'd and will be replaced by NMR package which is fully compatible with ZRB in terms of pinout and data sheet-equivalent electrical performance. Therefore, TM4C123BH6NMR is the new material to…