Part Number: TM4C123GH6PGE Other Parts Discussed in Thread: UNIFLASH , LMFLASHPROGRAMMER Hello Everyone!
We are trying to program tm4c123gh6pge on our custom board for a project which uses ADC and CAN.
At first we didn’t entered any clock setting and it…
Part Number: TM4C123GH6PGE I am utilizing a TM4C123GH6PGE microcontroller, which has a built-in hibernation module. However, I am not using this module in my application, and the MCU's datasheet only provides feedback concerning instances where the hibernation…
Part Number: TM4C123GH6PGE Other Parts Discussed in Thread: EK-TM4C1294XL Hi team,
The customer would like to know i s it possible to get the real time of the RTC from the M4(Year/month/day/hour/minute/second). If not, does the TI M4 have the capability…
Part Number: TM4C123GH6PGE Hi,
Currently we need test the board that using virtual port on TM4C123GH6PGET in win7 32bit platform.
May i know is there any driver that can support this?
regards,
TK
Hi Ayhan,
Glad that you got it working on PE5/PE4.
Ayhan Evren said: While examining the datasheet, I saw a table like this, where I noticed that the "Pin Assignment" of PF0 and PF3 is 3, not 8, unlike other pins. I wonder if this requires me to do something…
Part Number: TM4C123GH6PGE Other Parts Discussed in Thread: EK-TM4C1294XL
I'm using the TM4C123GXL launchpad to determine if the ARM M4 series microcontrollers will work for my application, which includes an SSI position encoder (iC-MU). The timing spec…
Part Number: TM4C123GH6PGE Hi team,
Using this M4 for SPI use, using oscilloscope for frequency and TX measurement, it is found that the waveform cannot be "square wave".
Causes the data resolution to be abnormal and the configuration is as…
Part Number: TM4C123GH6PGE Hi !
Excuse me but we had summer holidays..
But now we succeded in understanding exactly where we have the problem:
when UART1 TX (DMA channel 23) starts a burst trasmission with first byte START BIT synchronized with any…
Part Number: TM4C123GH6PGE Hello Everyone!
I am trying to enable internal pull-up resistors in the TM4C123GH6PGE on my custom board.
The purpose of this, I am addressing 10 multiplexers with PC 0-1-2-3 pins of the MCU. When I connected the Multiplexers…
Part Number: TM4C123GH6PGE Hi,
I have two sources for the timer4 CCP0 signal. So I like to switch between these two channels. At the TI HAL the function GPIOPinConfigure
exists. I don't see any GPIOPinConfigureReset or similar function.
This lead me…