Part Number: TM4C123GH6PZ Hi Champ,
I am asking for my customer.
They are trying to download with the device. The board was good before, but somehow, it is unable to download and with showing the error in below.
They have measured and compared the voltage…
Part Number: TM4C123GH6PZ Other Parts Discussed in Thread: TM4C123BH6PZ Hi Champs,
My customer wants to replace TM4C123 B H6PZ by TM4C123 G H6PZ. So far, I've only seen that the 2 ICs are different in operating temperature range only.
The new IC ( TM4C1…
Part Number: TM4C123GH6PZ Hi,
Good Day. I have a customer who is working with TM4C123GH6PZ. Please see below his query for your reference. Thank you very much.
Previously we have LM4F232H5QC for our application.
Now we are using TM4C123GH6PZ controller…
Part Number: TM4C123GH6PZ Hi team, helping a customer with this device. Thesoftware is bare metal with no operating system. They have a simple calculation of how much of the CPU bandwidth they are using. Getting too close to 100% utilization and they would…
Part Number: TM4C123GH6PZ Hi team,
We're working to implement a CAN stack to work with the TM4C123GH6PZ on top of the Tivaware Series C.
Is there 32 Message object per CAN controller, or 32 message objects total?
Thanks,
Jacob
Part Number: TM4C123GH6PZ Hello, Previously I asked a question about "unlock Jtag" with Tiva MCU,that is,we tried to unlock jtag by using our custom board and XDS100v2 but it failed. And the answer is ,there is a possibility that the Jtag circuit…
Part Number: TM4C123GH6PZ Hi, I can't find this register in TM4c123x datasheet, maybe there is an error in the errata.
workaround for #MEM03 from errata : Configure the external reset (RST) and the watchdog reset to issue a system reset (EXTRES = 0x2…
Part Number: TM4C123GH6PZ Hi TI,
I am designing a board with CAN communication based on the TM4C123GH6PZI. Attached is the wiring diagram.
Questions: 1-) Is the JTAG connection to connector P1 correct? 2-) Can I use in P1 a 5x2 connector with pitch 1.27…
Part Number: TM4C123GH6PZ Other Parts Discussed in Thread: UNIFLASH Hello,
I would like to ask a question about jtag access. I'm using TM4C123GGH6PZ on our custom board.
Previously I could load the program to TM4C123GGH6PZ by using CCSv6 or Uniflash…
Part Number: TM4C123GH6PZ Other Parts Discussed in Thread: TPS2051B Hi, I'm using tm4c123gh6pz on custom boards and programming them troguh usb port with LM flash programmer DFU and ROM bootloader and I getting some parts damaged or heated.
I have…