Part Number: TM4C129DNCPDT I have a warning message that persist so I decided to do something about it
#10247-D creating output section ". text" without a SECTIONS specification
In the EK_TM4C1294XL.cmd, the .text is already defined so not sure…
Part Number: TM4C129DNCPDT
Hi,
The MicroController is configured as USB Device. The board is self-powered.
With the initial Version we had a defect with the USB communication at customers site. We do not know what happend exactly.
By having a look into…
Part Number: TM4C129DNCPDT Please check if it is available of TM4C129 wake-up from deep sleep by CAN? Which clock setting or mode is available for the application and keeps minimum current consumption as possible?
Part Number: TM4C129DNCPDT We have a TIVA 129 configured with PLL frequency of 480MHz and system clock of 120 MHz. To reduce power at certain times, we wish to reduce the sysclk to a much lower value, while keeping everything else (including USB) operational…
Part Number: TM4C129DNCPDT https://e2e.ti.com/support/microcontrollers/other/f/908/t/834705
Hello team,
Previously I've asked about TDO toggle mechanism, see above history.
My customer returned a unit that I can observe the TDO toggle on them. However…
Part Number: TM4C129DNCPDT In TM4C129DNCPDT Data Sheet, Ethernet Controller module, MII Interface Signals, EN0TXER signal is allocated to PN6 (port N bit 6).
But TM4C129DNCPDT port N has only bit 0 to 5 as pin out.
There is an other signal allocated for…
Part Number: TM4C129DNCPDT Hi.
Currently, I meet one hard fault in SysCtlClockFreqSet() and I need to figure out the cause.
I have some information about this issue.
1. this issue can be reproduced by jumping to bootloader and hard fault occurred in …
Part Number: TM4C129DNCPDT Hi Tiva experts,
The datasheet mentioned that "if the device fails to initialization during reset, the hardware toggles the TDO output as an indication of failure."
My question is what kind of failure is that TDO able…
Part Number: TM4C129DNCPDT Hello everyone,
I'm using a TM4C129DNCPDT. One of the requirements of our project is to provide our users with the ability to update our firmware from the RS-232 port (UART0), the USB port (USB0), and a wireless module that…