Part Number: TM4C129ENCPDT Other Parts Discussed in Thread: TIDM-TM4C129POEAUDIO , , TPA3111D1 , OPA322 For our NVR project we need to make two separate Audio Boxes that will be connected with NVR over ethernet. This Box should be able to provide two way…
Part Number: TM4C129ENCPDT Can TM4C129ENCPDT handle both AES and DES simultaneously?
Is there any example that TI can provide doing AES and DES at the same time? Engineers in my organization tried and seems to not work and they doubt that the chip is…
Part Number: TM4C129ENCPDT I have a question. During serial connection on the USB0DM and USB0DP pins, a reset occurred several times, after which the surface temperature of the device became much higher than normal and the current consumption was also…
Part Number: TM4C129ENCPDT Dear expert,
I have some questions for TM4C129EN about the reference code part.
Do we have reference code for discrete Fourier transform?
Or there is other thing that means DFT code.
Best Regards,
Eric Chen
Part Number: TM4C129ENCPDT We have a function to call MAP_SysCtlReset() and it works most of the time.
Occasionally the processor hangs and doesn't reboot. We have to hit the reset pin to bring it back.
Our sequence in the function is to print a message…
Part Number: TM4C129ENCPDT Hi,
the following link seems no longer available: http://software-dl-1.ti.com/dsps/forms/vidtrackerMature.html and VID/PID for USB is needed.
Can you recommend another available link please?
Thanks,
Giorgia
Part Number: TM4C129ENCPDT
Hi,
I have configured the Internal ADC of the microcontroller. I am receiving correct values for AIN0, AIN1, AIN2, AIN3, however for AIN8 and AIN9 it would be spitting wrong values. I am guessing, if it has something to do with…
Part Number: TM4C129ENCPDT Other Parts Discussed in Thread: MSP432E401Y , Hello,
I am trying to implement the TM4C129ENCPDT circuit from the MSP432E401Y Launchpad. I was wondering if either the code or a binary for the XDS110 debugger is available for public…
Part Number: TM4C129ENCPDT Hey there, I'm fetching the time from pool.ntp.org, and it's used to update the time of the RTC, but due to some unknown issues, the updation is not working properly now. This is how I'm updating the RTC time,
void…
Part Number: TM4C129ENCPDT Hello Charles,
I hope you doing well.
I am facing another weird issue. I have two interrupts on GPIO_PORTM_BASE one is at GPIO_PIN_3 i.e. PM3 another is GPIO_PIN_6 i.e. PM6. GPIO_PIN_6 interrupt will always get triggered and land…