Part Number: TM4C129ENCPDT Hi Team,
Here's an issue from the customer may need your help:
I use the input capture function of the CCP pin to capture the rising edge of the 50Hz signal, and calculate the signal period based on the time difference between…
Part Number: TM4C129ENCPDT Other Parts Discussed in Thread: EK-TM4C1294XL Hi,
I need to enable uDMA for UART using the interrupt method. I am able to establish communication using the polling method, but when I move to the interrupt method, it doesn't…
Part Number: TM4C129ENCPDT Hello,
My objective is to establish a parallel communication bus between this MCU and an FPGA (Lattice Mach X02, or something similar). My design is using the EPI interface with the following configurations:
General Purpose…
Part Number: TM4C129ENCPDT Other Parts Discussed in Thread: UNIFLASH I am looking at old code that shows that we are attempting to do a factory reset of the TM4C by
1) Assert and hold the reset pin
2) Cycle the power
3) Initialize the JTAG port
4) Five…
Part Number: TM4C129ENCPDT Hi Everyone,
i am looking for the supportive documents for writing Bootloader for TM4C129ENCPDT under TI RTOS platform , where i like to place two differenr application in flash and select it using reset button during boot ,…
Hi Amit,
I have not heard back from you. I will close the thread for now. If you have any update you can write back here and the post will change its status to OPEN automatically.. I will suggest you use the scope to look at the DP and DM signals as…
Part Number: TM4C129ENCPDT Hi,
I'm working with a TM4C129ENCPDT microcontroller connected to external flash memory via SPI2. The connections are correct since it works when I use TI-RTOS. However, when I configure it without TI-RTOS, I can send data…
Part Number: TM4C129ENCPDT Other Parts Discussed in Thread: CC3100 , Hi Everyone,
I am searching for AWS embedded C sdk plugin for TM4C129ENCPDT where i am using TI RTOS with wifi chip CC3100 as well as ethernet, where can i find the AWS SDK for this ? …
Part Number: TM4C129ENCPDT Other Parts Discussed in Thread: SYSCONFIG Hello,
My project is based upon the tcpEcho project, which is included within the TI RTOS examples. I have successfully integrated both EPI and SPI functionality into the project (I…
Sahil said: I followed the link and made changes accordingly and it resolved the problem where the processor would stuck and we would loose the device and we had to use JTAG to reprogram the device locally. Now this problem is resolved.
Glad some progress…